How to disassemble a binary executable in yacto linux to get the assembly code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to disassemble a binary executable in yacto linux to get the assembly code?

ソリューションへジャンプ
19,136件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

I am using yacto with T4240 target and I built the u-boot.bin file. I want to check instruction.

Please provide command or path to generate assembly code from yacto linux executable binary.

SDK,

   QorIQ-SDK-V2.0-20160527-yocto

Regards,

VinothS

Regards,
Vinothkumar Sekar
ラベル(3)
0 件の賞賛
返信
1 解決策
5,322件の閲覧回数
vinothkumars
Senior Contributor IV

Hi,

I done 

<Yacto SDK installation directory>/build_t4240rdb-64b/tmp/sysroots/x86_64-linux/usr/bin/powerpc64-fsl-linux/powerpc64-fsl-linux-objdump -d u-boot-spl > u-boot-spl1.dis

u-boot-spl1.dis,

u-boot-spl: file format elf32-powerpc


Disassembly of section .text:

eff40000 <_start>:
eff40000: 27 05 19 56 dozi r24,r5,6486

eff40004 <version_string>:
eff40004: 55 2d 42 6f rlwinm. r13,r9,8,9,23

...................................................................

Regards,

VInothS

Regards,
Vinothkumar Sekar

元の投稿で解決策を見る

6 返答(返信)
5,322件の閲覧回数
Pavel
NXP Employee
NXP Employee

It looks like that this BSP does not supports this possibilities.

 

The simplest way for your task is CodeWarrior. CodeWarrior provides u-boot debugging and check instruction.

See the AN4876 application note:

https://www.nxp.com/docs/en/application-note/AN4876.pdf

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,323件の閲覧回数
vinothkumars
Senior Contributor IV

Hi,

I done 

<Yacto SDK installation directory>/build_t4240rdb-64b/tmp/sysroots/x86_64-linux/usr/bin/powerpc64-fsl-linux/powerpc64-fsl-linux-objdump -d u-boot-spl > u-boot-spl1.dis

u-boot-spl1.dis,

u-boot-spl: file format elf32-powerpc


Disassembly of section .text:

eff40000 <_start>:
eff40000: 27 05 19 56 dozi r24,r5,6486

eff40004 <version_string>:
eff40004: 55 2d 42 6f rlwinm. r13,r9,8,9,23

...................................................................

Regards,

VInothS

Regards,
Vinothkumar Sekar
5,322件の閲覧回数
Pavel
NXP Employee
NXP Employee

Yocto SDK provides generation u-boot source code. Disassembling is not needed for debugging.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,322件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Pavel,

In SDK after done built we got tool for binutils,

binutils includes objdump and libopcodes library for assembly code generation. 

By using this tool we can generate the assembly code for yacto linux executable. But, I don't know how to processed this and also I tried nothing I got.

<SDK installation directory>/build_t4160qds-64b/tmp/sysroots/t4160qds-64b/pkgdata/runtime-reverse u-boot-spl > u-boot-spl1.dis

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
5,322件の閲覧回数
Pavel
NXP Employee
NXP Employee

Usually the following command is used for u-boot code modification:

bitbake -c cleansstate u-boot

bitbake -c patch u-boot

This command generates source of the u-boot. See u-boot source using the similar path:

QorIQ-SDK-V2.0-20160527-yocto/build_t1042d4rdb/tmp/work/t1042d4rdb-fsl-linux/u-boot-qoriq/2016.01+fslgit-r0/git

 

Change u-boot code and use the following command for u-boot building:

bitbake -c compile -f u-boot

bitbake u-boot

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,322件の閲覧回数
vinothkumars
Senior Contributor IV

Hi Pavel,

Thank you for your reply.

Whatever you mentioned commands are the general for building/compiling purpose.

After compilation we got linux executable binary file by using this file we can generate disassembly code file for u-boot debugging.

For this purpose. there is specific tool under the yacto sdk.

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信