How to apply a customer patch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to apply a customer patch

1,430件の閲覧回数
junjieshi
Contributor I

Hi,

I am using the 'QorIQ-SDK-V2.0-20160527-yocto' for T4240RDB, to build a 'fsl-image-minimal'. I am trying to apply a patch for the linux kernel. How can I apply the patch and make the menuconfig? I have tried to modify the recipes under 'source/poky/meta/recipes-kernel/linux', to add the one line: 'SRC_URI += "file://patch.patch". However, it doesn't work. Is there anyone knows how to make it possible?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,228件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Section 3.3.3 of NXP SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信