Hardware Design Considerations for T1040

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware Design Considerations for T1040

1,389 Views
mohsenhaghighat
Contributor III

Hi,

I want to design a board with T1040 Processor.Do any PDFs or information about Hardware Design Considerations of T1040 exist?

Thanks

Labels (1)
1 Reply

1,137 Views
alexander_yakov
NXP Employee
NXP Employee

We do not offer "Reference Schematics" for our processors, but we offer development boards based on our processors, and offer full board design collateral for these boards for your reference. Here is a direct link to T1040 RDB board product page, where you can find schematic and use it as reference for your design:

QorIQ T1040 Reference Design Board|NXP

For hardware design considerations please look "T1040 Family Design Checklist" (application note AN4825). This document is available for download from T1040 Documentation page:

QorIQ T1040 and T1020 Multicore Communications Proc|NXP

Please feel free to ask further questions in this community and y creating a direct requests to NXP online technical support.

How I could create a Service Request?

Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------