Fman microcode version for T1040RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fman microcode version for T1040RDB

1,879件の閲覧回数
suchitasharma
Contributor I

Hi,

      I am using T1040 processor  with silicon version is 1.1 and using fsl_fman_ucode_t1040_r1.1_107_4_2.bin.

 

I have noticed that the clock frequencies for QE ,FMAN,QMAN & PME are  different (lesser)  from the frequencies mentioned in T1040RDB documentation. And when performing throughput test i have noticed significant reduction in packet sizes.Please suggest the correct fman microcode version which needs to be fused in T1040rdb processor / suggest alternate solution. 

The Uboot initialization log is as shown below.

U-Boot 2014.07 (Apr 22 2020 - 12:01:10)

CPU0: T1040E, Version: 1.1, (0x85280011)
Core: e5500, Version: 2.1, (0x80241021)
Clock Configuration:
CPU0:1400 MHz, CPU1:1400 MHz, CPU2:1400 MHz, CPU3:1400 MHz,
CCB:400 MHz,
DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:33.333 MHz
QE:200 MHz
FMAN1: 400 MHz
QMAN: 200 MHz
PME: 200 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 0818000e 0e000000 00000000 00000000
00000010: 69000002 80000002 ec027000 21000000
00000020: 00000000 00000000 00000000 0001a000
00000030: 00000000 00225a8f 00000000 00000000

0 件の賞賛
返信
1 返信

1,871件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please use the attached FMAN ucode.

_106_
This IRAM package includes the following main features:
Custom Classification (CC), Independent-Mode (IM),
Host-Commands (HC), IPv4/6 Fragmentation (IPF),
IPv4/6 Reassembly (IPR), IPsec and Header Manipulation (HM).
Release Notes: DPAA_IPACC_ReleaseNote.pdf

_107_
This IRAM package includes the following main features:
Custom Classification (CC), Independent-Mode (IM),
Host-Commands (HC) and Deep Sleep Auto Response (DSAR).
For DSAR the following features are supported: ARP, ICMP, ND and SNMP.
Release Notes: DPAA_DSAR_ReleaseNote.pdf

_108_
This IRAM package includes the following main features:
NG CAPWAP, Custom Classification (CC), Independent-Mode (IM),
Host-Commands (HC), IPv4/6 Fragmentation (IPF),
IPv4/6 Reassembly (IPR), IPsec and Header Manipulation (HM).
Relese Notes: DPAA_NG_CAPWAP_ReleaseNote.pdf

 

CC IM HC IPF IPR HM DSAR CAPWAP
106 + + + + + + - -
107 + + + - - - + -
108 + + + + + + - +

0 件の賞賛
返信