Flash programming Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash programming Issue

1,402 Views
abhishekborana
Contributor II

Hii...  Is it possible to have complete code (RCW, PBI and UBoot) only in SPI ? Can I boot from SPI Flash alone without using any IFC memory ?  Also I am not able to program NOR flash  of a new custom board based on T1024. What can be the reason ? 

Tags (2)
0 Kudos
Reply
1 Reply

1,340 Views
ufedor
NXP Employee
NXP Employee

> Is it possible to have complete code (RCW, PBI and UBoot) only in SPI ?

Yes.

You could find pre-built U-Boot SPI images in the QorIQ Linux SDK v2.0 PPCE5500 IMAGE ISO freely available at:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7726177 

> Can I boot from SPI Flash alone without using any IFC memory ? 

Yes.

> Also I am not able to program NOR flash  of a new custom board based on T1024. What can be the reason ? 

Please created separate question.

0 Kudos
Reply