FMAN µCode for T2081

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FMAN µCode for T2081

跳至解决方案
2,442 次查看
ralftruebenbach
Contributor III

Hello,

which fman µcode do I have to use for the T2081? Is "QorIQ Linux SDK v2.0 PPC64E6500 IMAGE.iso/t2080qds-64b/fsl_fman_ucode_t2080_r1.1_108_4_5.bin" from QorIQ Linux SDK correct?

Kind regards,

Ralf

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,101 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

The T2080 and T2081 has the same FMAN, so customer can use the ucode for both devices. There are two T2080 microcodes – _106_ and _108_. You can look for its features in

http://git.freescale.com/git/cgit.cgi/ppc/sdk/fm-ucode.git/tree/readme?id=fsl-sdk-v2.0

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,102 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

The T2080 and T2081 has the same FMAN, so customer can use the ucode for both devices. There are two T2080 microcodes – _106_ and _108_. You can look for its features in

http://git.freescale.com/git/cgit.cgi/ppc/sdk/fm-ucode.git/tree/readme?id=fsl-sdk-v2.0

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复