ETHERNET T1042

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ETHERNET T1042

1,724 Views
gokulkrishnan
Contributor III

Hi,

I am using the T1042 processor for my design. In this I am not using the EC2 RGMII section. So if I don't need to program it as an output can I leave it as unconnected?

Regards 

Gokul

Labels (1)
Tags (1)
1 Reply

1,563 Views
alexander_yakov
NXP Employee
NXP Employee

If you are not using EC2 RGMII in your design, unused EC2 RGMII pins should e terminated as recommended in T1040 family Design Checklist (application note AN4825), Table 20, Section "EC2 in RGMII mode".

This document is available for download from T1042 Product Page, "Documentation" tab:

QorIQ® T1042 and T1022 Multicore Communications Processors|NXP 


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply