Does the T1014 L1 and L2 cache have ECC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the T1014 L1 and L2 cache have ECC?

1,041件の閲覧回数
raymondhaas
Contributor I

We are evaluating the T1014 processor for a new product.  I know that the external DDR3 memory supports ECC.  However does the L1 and L2 cache used by the e5500 core have ECC or parity?

ラベル(1)
0 件の賞賛
返信
1 返信

875件の閲覧回数
ufedor
NXP Employee
NXP Employee

L1

Data Cache has 1 parity bit/byte and 1 parity bit/tag.

Instruction cache has 1 parity bit/word and one parity bit/tag.

L2

Configurable ECC or parity protection for data array and parity protection for tag array

Please refer to the e5500 Core Reference Manual for additional details:

https://www.nxp.com/webapp/Download?colCode=E5500RM

0 件の賞賛
返信