Debug Register(debug_29) is not present

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug Register(debug_29) is not present

2,570 Views
vinothkumars
Senior Contributor IV

Hi All,

I got Automatic Calibration Error (ACE) when doing DDR initialization and I got this thread and followed this thread,

T4240 DDR initialize: why pops out "Automatic calibration error" in the DDRx_ERR_DETECT? 

According to this thread, there is a debug_29 register for changing data rate for debugging purpose to avoid this types of ACE error.

But, I never see debug_29 register for t4240 target from T4240RM.pdf reference manual.

Please clarified my doubt.  

Thanks, VinothS

Regards,
Vinothkumar Sekar
Labels (1)
0 Kudos
Reply
4 Replies

2,335 Views
ufedor
NXP Employee
NXP Employee

For this erratum DEBUG_29 is at CCSRBAR + DDR_OFFSET + f70h.

0 Kudos
Reply

2,335 Views
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply. 

So, I will use the debug_29 register in ddr initialization.

Is it right?

ex:

   debug_29 = 0x00700064

   (or)

   Data.Set ANC:CCSRBAR + DDR_OFFSET + f70h %Long %BE 0x00700064 ; In Lauterbach Script

Thanks, VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply

2,335 Views
ufedor
NXP Employee
NXP Employee

Which processor you are using?

> Data.Set ANC:CCSRBAR + DDR_OFFSET + f70h %Long %BE 0x00700064 ; In Lauterbach Script

Sorry, we do not use the Lauterbach tools - please check with Lauterbach directly.

Please consider that there could be other causes of the ACE been set - for example:

a) DDR SDRAM reset not applied or has incorrect timing

b) DQ mapping for DDR4 SDRAM is incorrect

c) incorrect PCB layout

Usually it is convenient to investigate the ACE issue as Technical Case:

1)    open www.nxp.com
2)    Select "Support" -> "All Support Options"
3)    Click "Go to Tickets"
4)    Log in with your NXP login and password
5)    On the "Group, Create and View your support cases" page press "+ Add a new case" to start the process.

0 Kudos
Reply

2,335 Views
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your quick reply.

I am using T4160rdb processor.

VInothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply