DPAA Frame Queue Rules

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DPAA Frame Queue Rules

2,261 Views
michayardeny
Contributor III

DPAA question - I'm using t1042 QorIQ.  

In the former platforms etsec had a filer mechanism that defined what goes to a specific  Frame Queue. With the DPAA I'm looking at the FQD table and I don't understand what is the mechanics for specific data frame from a port (memac for example) to be enqueued to a specific frame queue?

Am I missing something ?

Thanks Micha

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

2,050 Views
bpe
NXP Employee
NXP Employee


Compared to eTSEC, DPAA implements much more complex flows to define the target Frame Queue for a frame. Several flows and decision mechanisms can be
configured. Refer to  T1040DPAARM, Sections 5.3.19.1, 5.10, 5.13 for details.

Have a great day,

Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,050 Views
michayardeny
Contributor III

Frame manager is the entity that defines rules for the input frames.

0 Kudos
Reply