DDR Initialization using CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Initialization using CodeWarrior

Jump to solution
2,944 Views
vinothkumars
Senior Contributor IV

Hi,

I am working on t4160 board and I want to initializae DDR and test memory. I followed this document and I not clear that. 

Will you please provide the steps or verify my steps right or wroung?

Reference Link: 

http://cache.freescale.com/files/training/doc/ftf/2014/FTF-NET-F0137.pdf

Steps:

1. Open CodeWarrior Flashprogrammer

2. Go to Hardware Diagnostics Action for DDR initialization
Run->Debug Configuration->Edit Harware->Initialization File->select T4160qds_init_Core.tcl

3. Create a New Task
Click-> Create a New Task->select Hardware Diagnostic as Task Type -> Finish

4. Go to Hardware Diagnostics Action for Memory Test
Select Memory Test->check(Walking 1's, Bus Noise and Address)

5. Stat run

6. Once done the ddr initialization open debug shell and run the following commands,
"display 0x000 20"

Thanks, VinothS

Regards,
Vinothkumar Sekar
Labels (1)
0 Kudos
Reply
1 Solution
2,737 Views
ufedor
NXP Employee
NXP Employee

The Hardware Diagnostics Actions (including Memory tests) are described in detail in the CodeWarrior Development Studio for Power Architecture Processors Targeting Manual (Targeting_PA_Processors.pdf), 11.3 Hardware diagnostics.

View solution in original post

0 Kudos
Reply
2 Replies
2,738 Views
ufedor
NXP Employee
NXP Employee

The Hardware Diagnostics Actions (including Memory tests) are described in detail in the CodeWarrior Development Studio for Power Architecture Processors Targeting Manual (Targeting_PA_Processors.pdf), 11.3 Hardware diagnostics.

0 Kudos
Reply
2,737 Views
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply

Regards, VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply