Could not connect to probe(or other debug links). CC string is invalid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Could not connect to probe(or other debug links). CC string is invalid

3,536 次查看
athershehzad
Contributor III

I am trying to flash my T1042RDB based custom board using Code warrior tap. When I connect my codewarrior tap to my PC, Green LED starts blinking that shows the connectivity of PC and Codewarrior tap. I am also able to see my freescale probe in device manager but it is not shown in the notification tray. When I starts flashing, it gives the error that

Connection failed.

Could not connect to probe [or other debug link]. CC string is invalid.

What might the reason for this error ?

标签 (1)
标记 (2)
0 项奖励
回复
6 回复数

3,289 次查看
athershehzad
Contributor III

Sir Is there any other way by which I can configure my Codewarrior Tap by myself ?

0 项奖励
回复

3,289 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ather Shehzad,

The problem should be caused by the unstable hardware, please return it for a new TAP.

Thanks,

Yiping

0 项奖励
回复

3,285 次查看
athershehzad
Contributor III

Thanks Yiping Wang
You might be right because when I enter show cc it gives me error
0: USB open failure

but sometimes it gives me the expected result

0: CodeWarrior TAP (cwtap) CC software ver. {0.0}

Yes Code warrior is shown in device manger that can be seen in the attachment below

What is the solution to the usb connection issue ?

Regards

0 项奖励
回复

3,285 次查看
yipingwang
NXP TechSupport
NXP TechSupport

It's seems that the hardware of your CodeWarrior TAP is not stable, please contact your local FAE to return and replace it with new one.

0 项奖励
回复

3,285 次查看
athershehzad
Contributor III

Is there any other way to configure the CodeWarrior hardware by ourself ?

Regards,

0 项奖励
回复

3,283 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ather Shehzad,

It seems that there is problem to detect CodeWarrior TAP with USB connection.

Please open CodeWarrior Connection Sever to check whether CodeWarrior information can be returned correctly.

(bin) 2 % config cc cwtap
(bin) 3 % show cc
0: CodeWarrior TAP (cwtap) CC software ver. {0.0}

In addition, please check whether CodeWarrior TAP can be detected as the attachment from the device manager.

Thanks,

Yiping

0 项奖励
回复