Hi,
I would like to modify uboot variables from Linux. Is this possible? I have seen that it is possible to compile the kernel with some options in order to be able to access to them, but I cannot seen this option.
Target filesystem options ---> [*] Das U-Boot Boot Monitor ---> [*] fw_printenv tool in target
Best regards
解決済! 解決策の投稿を見る。
Hello manolo ruiz ,
I assume you use SDK 2.0, please refer to the following procedure.
Please add "u-boot-fw-utils" into variable IMAGE_INSTALL_append in meta-freescale/recipes-fsl/images/fsl-image-core.bb.
And run "bitbake fsl-image-core" to rebuild this tool into filesystem.
On the target board, please create a configuration file /etc/fw_env.config, the content like this
/dev/mtd5 0x60000 0x2000 0x100000
MTD device name
Device Offset
Environment Size
Flash sector size
Then execute "fw_printenv" and "fw_setenv" to read and write u-boot environment.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello manolo ruiz ,
I assume you use SDK 2.0, please refer to the following procedure.
Please add "u-boot-fw-utils" into variable IMAGE_INSTALL_append in meta-freescale/recipes-fsl/images/fsl-image-core.bb.
And run "bitbake fsl-image-core" to rebuild this tool into filesystem.
On the target board, please create a configuration file /etc/fw_env.config, the content like this
/dev/mtd5 0x60000 0x2000 0x100000
MTD device name
Device Offset
Environment Size
Flash sector size
Then execute "fw_printenv" and "fw_setenv" to read and write u-boot environment.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I performed these steps using the QorIQ SDK v2.0 and received the following errors:
$ bitbake fsl-image-core
Loading cache: 100% |########################################################################################################################################| ETA: 00:00:00
Loaded 3437 entries from dependency cache.
Parsing recipes: 100% |######################################################################################################################################| Time: 00:00:00
Parsing of 2733 .bb files complete (2729 cached, 4 parsed). 3438 targets, 248 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'u-boot-fw-utils' (but /LS1020A/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb RDEPENDS on or otherwise requires it)
ERROR: u-boot-fw-utils was skipped: Only config,images can be specified!
NOTE: Runtime target 'u-boot-fw-utils' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['u-boot-fw-utils']
ERROR: Required build target 'fsl-image-core' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-core', 'u-boot-fw-utils']
Does anyone know how to fix this?
Thanks for your answer. Is the answer also valid for SDK 1.9 and 1.8?
Best regards,
Manolo.
Yes, it is valid for SDK 1.9 and 1.8.
Thanks,
Yiping
Hi Manolo,
Yes you can access u-boot variables over Memory technology Device Layer (MTD). For detailed information you can see here HowCanIAccessUBootEnvironmentVariablesInLinux < DULG < DENX
Michal