Build Minimal u-boot binary for t4160rdb board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build Minimal u-boot binary for t4160rdb board

ソリューションへジャンプ
1,589件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

I am using t4160rdb board with Lauterbach. Now this board have ddr controller issue. So, I want to flash into sram. because of this, I built the minimal image ( secondary program loader (spl))

Now, I have the doubt, 

I built this binary by setting T4240RDB_SDCARD_defconfig in machine configuration file. And I check u-boot  code CONFIG_SDCARD macro also set. 

Is it possible to flash u-boot-spl.bin (160 KB) through the NOR flash into SRAM ?

If it not, why ? or if it yes, how?

If it possible, please provide steps to build minimal u-boot for NOR flash

Regards,

VinothS

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
1 解決策
1,429件の閲覧回数
bpe
NXP Employee
NXP Employee

I guess you answered to yourself:

https://community.nxp.com/thread/494805 

Please avoid creating multiple discussion threads for a single technical issue.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,430件の閲覧回数
bpe
NXP Employee
NXP Employee

I guess you answered to yourself:

https://community.nxp.com/thread/494805 

Please avoid creating multiple discussion threads for a single technical issue.

0 件の賞賛
返信
1,429件の閲覧回数
vinothkumars
Senior Contributor IV

Hi bpe,

Will you please clarify the following,

1. Is SPL image support NOR flash ?

2. If it no, what configuration I want to do?

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
1,429件の閲覧回数
vinothkumars
Senior Contributor IV

Finally,

I clarified Secondary Boot Loader (SPL) is loaded by NAND flash

Regards,
Vinothkumar Sekar
0 件の賞賛
返信