Auto script calling in t2080rdb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Auto script calling in t2080rdb

2,526 Views
vidyasagartata
Contributor II

Dear All,

I am following below steps to call auto script in T2080RDB.

1).cd /etc/init.d

2).vi helloworld.sh

#!/bin/sh   

echo ""echo "Hello from user!!!"echo ""

3).chmod +x helloworld.sh

4).cd /etc/rc5.d

ln -s ../init.d/helloworld.sh S99helloworld

Then reboot the t2080rdb but linux log does not show Hello from user!!!

Thanks,

Vidya

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

2,083 Views
vidyasagartata
Contributor II

Dear Pavel,

Yes we are getting, we are using jffs2 file system but after enabling auto script error through "jffs2: Empty flash at 0x0234fffc ends at 0x02350000" many times.

Please tell me what is the issue.

Thanks,

Vidya

0 Kudos
Reply

2,083 Views
Pavel
NXP Employee
NXP Employee

I have tested your modified command sequence. See below:

cd /etc/init.d

vi helloworld.sh

 

ls

banner.sh     functions                 inetd.busybox         rc                        sendsigs        syslog.sysklogd

bootlogd      functions.initscripts     modutils.sh           rcS                       single          udev

bootmisc.sh   functions.lsbinitscripts  mountall.sh           read-only-rootfs-hook.sh  sshd            udev-cache

busybox-cron  halt                      mountnfs.sh           reboot                    stop-bootlogd   umountfs

checkroot.sh  helloworld.sh             netperf               rmnologin.sh              sysfs.sh        umountnfs.sh

devpts.sh     hostname.sh               networking            run-postinsts             syslog          urandom

dmesg.sh      hwclock.sh                populate-volatile.sh  save-rtc.sh               syslog.busybox  xinetd

/etc/init.d# chmod +x helloworld.sh

 

./helloworld.sh

echo Hello from user!!!echo

 

cd /etc/rc5.d

ln -s /etc/init.d/helloworld.sh S99helloworld

 

ls

S01networking  S15mountnfs.sh  S20netperf  S20xinetd      S99rmnologin.sh

S09sshd        S20hwclock.sh   S20syslog   S99helloworld  S99stop-bootlogd

 

./S99helloworld

echo Hello from user!!!echo

Check also your root file system.

Are there S99helloworld and helloworld.sh files after reboot.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply