floating license  failed!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

floating license  failed!

Jump to solution
3,724 Views
gaokui
Contributor I

1、floating license的安装问题(CW_S12_v5.1开发环境)

2、首先在官网上面先生成lincese.dat文件,生成方法我是参考文档《Software and Support Activation Quick Start Guide》,具体步骤如下:

146772_146772.pngpastedImage_5.png

146773_146773.pngpastedImage_6.png

单击generate,生成lincese

146774_146774.pngpastedImage_7.png

单击save all,保存生成的lincese.dat文件

3、安装FSLFlexLMinstall管理程序,我参考的文档是《Floating License Installation Guide for Windows》,具体步骤如下:

进入许可管理器的网站

 

146776_146776.pngpastedImage_12.png

我所使用的服务器版本,

146777_146777.pngpastedImage_13.png

服务器上准备好安装必须文件,

146779_146779.pngpastedImage_15.png

开始安装许可管理程序

146780_146780.pngpastedImage_16.png

安装完成之后,运行

146781_146781.pngpastedImage_17.png

146782_146782.pngpastedImage_18.png

单击start server

146786_146786.pngpastedImage_21.png

 

 

客户机上安装环境变量

146785_146785.pngpastedImage_20.png

客户机上安装CW_S12_V5.1,下载安装包文件

146787_146787.pngpastedImage_22.png

下载完成后,开始安装,安装完成之后,IDE打开,显示没有注册,

146788_146788.pngpastedImage_23.png

 

同时在服务器上面

146789_146789.pngpastedImage_24.png

红色框图显示的完整信息如下

--------

Status

--------

Flexible License Manager status on Tue 4/26/2016 09:33

 

 

[Detecting lmgrd processes...]

License server status: [email protected]

    License file(s) on 192.168.10.253: C:\FSL_FlexLM\license.dat:

 

 

192.168.10.253: license server UP (MASTER) v11.5

 

 

Vendor daemon status (on 192.168.10.253):

 

 

  metrowks: UP v11.5

Feature usage info:

 

 

Users of HI100360:  (Total of 1 license issued;  Total of 0 licenses in use)

 

 

Users of HI407284:  (Total of 1 license issued;  Total of 0 licenses in use)

 

 

Users of HI100300:  (Total of 1 license issued;  Total of 0 licenses in use)

 

 

Users of ProcessorExpertHCS12:  (Error: 1 licenses, unsupported by licensed server)

 

 

Users of Win32_CWIDE_Unlimited:  (Error: 1 licenses, unsupported by licensed server)

 

 

Users of HI100350:  (Total of 1 license issued;  Total of 0 licenses in use)

 

 

 

问题:为什么客户机上IDE没有注册?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,058 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello gao

First, please place the license file under CodeWarrior installation folder, usually is: C:\Program Files\Freescale\CWS12v5.1

Then, please check the hard disk ID of your server,  to get it, please:

  1.       Open a DOS prompt
  2.       Type ‘cd C:’ (return
  3.       Type ’VOL’ (return)
  4.       Copy the Volume Serial Number value without the dash

For how to install Floating license, please refer to this doc:

http://www.freescale.com/files/soft_dev_tools/doc/user_guide/CW_FLOA_LICEN_UG.pdf

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,059 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello gao

First, please place the license file under CodeWarrior installation folder, usually is: C:\Program Files\Freescale\CWS12v5.1

Then, please check the hard disk ID of your server,  to get it, please:

  1.       Open a DOS prompt
  2.       Type ‘cd C:’ (return
  3.       Type ’VOL’ (return)
  4.       Copy the Volume Serial Number value without the dash

For how to install Floating license, please refer to this doc:

http://www.freescale.com/files/soft_dev_tools/doc/user_guide/CW_FLOA_LICEN_UG.pdf

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply