codewarrior license

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior license

Jump to solution
15,119 Views
moti
Contributor I
Hi!
i recived a license and I dont know in what directory to put it?!
I reced an 202049 error about licence!!
what 2 do??
thank u!
 
Labels (1)
0 Kudos
Reply
1 Solution
5,444 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi there,

the process has 2 phases:

www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LICENSE

the second point allows you to activate your license, provide the required information and the licensing department will send you an evaluation license file.

Note: the linux tools per default come with and empty license.dat file... nothing to do with the licensing process, nothing to be worry about.

Hope this helps...

Regards


View solution in original post

0 Kudos
Reply
6 Replies
5,445 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi there,

the process has 2 phases:

www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LICENSE

the second point allows you to activate your license, provide the required information and the licensing department will send you an evaluation license file.

Note: the linux tools per default come with and empty license.dat file... nothing to do with the licensing process, nothing to be worry about.

Hope this helps...

Regards


0 Kudos
Reply
5,444 Views
Alban
Senior Contributor II
Hello Moti,

The license.dat file goes into the root of your CodeWarrior installation.

For instance: C:\Program Files\Freescale\Codewarrior for HC12 V4.6\license.dat

Cheers,
Alban.
0 Kudos
Reply
5,444 Views
Enlighten_me
Contributor I
 Hi,
      I have just installed CodeWarrior Development Studio, Linux platform - Evaluation. On running the CodeWarriorIDE I receive the following error message :-

No valid license key was found for this installation of
CodeWarrior Development Studio. Please register
your product by following the instructions on the
registration card or by contacting [email protected] or (800) 377-5416.

A blank license file was installed when I installed the software ?, I registered the evaluation copy via the Internet., but this just provided me with an activation key. Can you tell me why the license.dat file is blank ? and what can I do in order to be able to use this software ?

Thanks in advance,

0 Kudos
Reply
5,444 Views
Enlighten_me
Contributor I
Hi Voxan,
                Thanks for your help, I have already activated my license but I have not received any evaluation license file for the licensing department.
 
Regards,
 
Enlighten_me
0 Kudos
Reply
5,444 Views
hehe_336
Contributor I

Hi!

      I'm one user of codewarrior for coldfire v6.3, registered for a long time. However, I haven't receiced the license code. Can you told me how you activated your license. Thank you!

0 Kudos
Reply
5,444 Views
CrasyCat
Specialist III

Hello

 

I checked CRM.

Apparently your Entitlement ID starts with AAZB. Am I correct?

 

This one is associated with Codewarrior Development Studio, ColdFire Special Edition.

 

With this entitlement you do not need to activate your license. Special edition license file should be installed with the tool chain.

 

CrasyCat

0 Kudos
Reply