co-developing model

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

co-developing model

2,993 Views
tommasomagnani
Contributor I

we got a CodeWarrior floating license that we would share with an external developer for a new project in co-developing model, is it possible in according to EULA?

Labels (1)
4 Replies

2,651 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello TommasoTommaso Magnani

The Borrowing feature of the floating licenses allows users to ‘borrow’ a license

from the floating license server for a limited time, disconnect from the network and to use

the borrowed license even with no connection to the license server. For how to use it, you may refer to this thread:

https://community.freescale.com/thread/389440

Or you can contact us to get a temporary license. To submit a case, please refer to:

https://community.freescale.com/docs/DOC-330215

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,651 Views
tommasomagnani
Contributor I

Hello Fiona,

I know that feature, but my question is about License, the EULA states:

"You may not rent, lease, sublicense, lend or encumber the Software,

unless otherwise expressly agreed to within this Agreement", in my

scenario we have to buy a new license to external developer? Or he can

"borrows" our license to develop in our team?

Best Regards

Tommaso

0 Kudos
Reply

2,652 Views
TomasPaez
NXP Employee
NXP Employee

Hi Tommaso, here my comment,

This action item is for your own development project , right ? so I understand you are not leasing, renting the suite to your contractor or getting any profit from the suite use, since development is for your project, you are OK.

0 Kudos
Reply

2,651 Views
TomasPaez
NXP Employee
NXP Employee

It is possible, just keep mind your license support a certain amount of seats.

The number of seats will determine how many user can run the tool in a specific time, make sure you do not exceed this number.

Hope this helps.

Regards.

0 Kudos
Reply