can I use CodeWarrior after registration expires?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

can I use CodeWarrior after registration expires?

跳至解决方案
1,349 次查看
danielmilutinov
Contributor III

Hi,

 

I am programming in assembly and my CodeWarrior 30-day evaluation period is about to expire. My understanding is that I can continue to use CodeWarrior after the 30 period and don't need to do anything, even though the pop-up screen says I can use CodeWarrior until the current license expires. 

 

Please confirm.

 

Dan

标签 (1)
0 项奖励
回复
1 解答
1,226 次查看
danielmilutinov
Contributor III

CodeWarrior continues to function normally after the 30-day evaluation period, so there is no need to register. 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,226 次查看
stanish
NXP Employee
NXP Employee

Hello Daniel,

Not sure which CodeWarrior you are using.

Usually after the evaluation period expires it is automatically switched to free Special Edition (if such version exists) so you don't have to register it.

Stan

0 项奖励
回复
1,227 次查看
danielmilutinov
Contributor III

CodeWarrior continues to function normally after the 30-day evaluation period, so there is no need to register. 

0 项奖励
回复