Using USB Dongle with Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using USB Dongle with Linux

Jump to solution
2,398 Views
caryo_brien
Contributor III

We purchased a node locked CodeWarrior and a USB Dongle.  We do all

our development in Linux.

 

a) Will the USB Dongle work with Linux hosts?

 

b) How do I get the USB Dongle ID on a Linux host?  The instructions

are only for windows.

 

Cary O'Brien

Labels (1)
0 Kudos
Reply
1 Solution
2,168 Views
trytohelp
NXP Employee
NXP Employee

Hi Cary,

Unfortunately the USBDongle is not running on Linux OS.

We don't have driver running on Linux.


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,168 Views
trytohelp
NXP Employee
NXP Employee

Hi Cary,

Unfortunately the USBDongle is not running on Linux OS.

We don't have driver running on Linux.


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply