[Q] v11.0 C++ build error with Prof. license

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Q] v11.0 C++ build error with Prof. license

1,220 Views
jongcheonkim
Contributor II

Hello. I have CodeWarrior Prof. license

I tested with CodeWarrior for MCU v11.0

- C++ project with Volume ID license generate: no problem

- C++ project with USB Dongle ID license generate: 'C++ is not supported by the current set of licenses and is disabled.'

  error happen.

(I checked license activate via CodeWarrior and LMTOOLS both)

- C project: no problem regardless of Volume ID/USB Dongle ID license

For CW to v10.7 with same USB Dongle.

I have no problem C++ project - license gen via Dongle ID

What do I need to check to use CW v11.0 via Dongle License?

Best Regards,

Mac.

0 Kudos
Reply
1 Reply

1,102 Views
jongcheonkim
Contributor II

Hello.

I accidentally pressed the 'assumed answer' button, but this issue has not been resolved yet. ;-(

If you know the solution, please answer it.

Best Regards,

Mac.

0 Kudos
Reply