Programming without license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming without license

ソリューションへジャンプ
8,076件の閲覧回数
rdazcal
Contributor III

Greetings,

 

I have developed a firmware for a CF-V2 on the CW7.2 platform and intend to develop a second one.

 

But on this second one, it was requested that the support team need to be able to re-program the devices on field if a FW update is required.

 

Since my code exceeds Freescale's free license limitation, I have bought a floating license to use here in the company.

 

But on the field that will not be a possibility.

 

It seems my only option is to provide the support team with a Cyclone MAX stand alone programmer, but that means $900 per support team, which is a LOT.

 

Isn't there any other option for me? What about CW10? Does it have a higher size limitation than CW7.2 for the CF-V2 family?

 

Thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
7,726件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

CFFlasher is a good option together with P&E BDM. It will not disturb any other programs.

 

The uTasker project includes boot loaders for the CF V2 parts - USB, serial and Ethernet, depending on what the parts has, included encrypted loading support for working with chips with protected FLASH settings. See www.uTasker.com

 

Regards

 

Mark

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
7,726件の閲覧回数
scifi
Senior Contributor I
0 件の賞賛
返信
7,726件の閲覧回数
rdazcal
Contributor III

Thanks scifi...

 

How safe is it to install CF Flasher?

 

Can it affect my current CW7.2 functionality?

0 件の賞賛
返信
7,726件の閲覧回数
scifi
Senior Contributor I

 


rdazcal wrote:

How safe is it to install CF Flasher?

Can it affect my current CW7.2 functionality?


To be honest, I don't know. In theory, it shouldn't. Obviously, if you try to use the BDM adapter simultaneously with CW and CF Flasher, some kind of conflict may occur.

 

0 件の賞賛
返信
7,727件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

CFFlasher is a good option together with P&E BDM. It will not disturb any other programs.

 

The uTasker project includes boot loaders for the CF V2 parts - USB, serial and Ethernet, depending on what the parts has, included encrypted loading support for working with chips with protected FLASH settings. See www.uTasker.com

 

Regards

 

Mark

 

 

0 件の賞賛
返信
7,726件の閲覧回数
TomE
Specialist II

Can you change the device to program itself from Ethernet, USB or a serial port?

 

0 件の賞賛
返信
7,726件の閲覧回数
rdazcal
Contributor III

Hi Tom,

 

Making it program it self will be quite tricky... although it's definetly a goal for the near future.

 

Do you know if there is code size limitation in CW10 for programming on the free license?

 

0 件の賞賛
返信
7,726件の閲覧回数
J2MEJediMaster
Specialist I

Size limit for the Special Edition of CW v10 for MCUs, in regard to ColdFire V2 programs, is 128KB.

 

---Tom

0 件の賞賛
返信