Lmcrypt error when generation CW key

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lmcrypt error when generation CW key

3,336件の閲覧回数
peder77
Contributor I

Hi

 

I'm trying to generate a CW key but gets an error "The call to lmcrypt failed", what to do?

 

126818_126818.pngClipboard01.png

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,037件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Peter, David,

I performed some tests on my side under my NXP account and a hotmail account.

I can generate the license file without problem for different products.

For HC12

pastedImage_0.png

For MCU V10.6

pastedImage_1.png

Can you try again ?

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,037件の閲覧回数
peder77
Contributor I

For some reason it now works...

0 件の賞賛
返信

3,037件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Peder,

It seems the problem was solved

Pascal

0 件の賞賛
返信

3,037件の閲覧回数
d_li
Contributor III

I am also getting the same error as well. :smileyconfused:

0 件の賞賛
返信