Linux evaluation software licensing problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux evaluation software licensing problems

ソリューションへジャンプ
3,445件の閲覧回数
Enlighten_me
Contributor I
  Hi,
      I have just installed CodeWarrior Development Studio, Linux platform - Evaluation. On running the CodeWarriorIDE I receive the following error message :-

No valid license key was found for this installation of
CodeWarrior Development Studio. Please register
your product by following the instructions on the
registration card or by contacting [email protected] or (800) 377-5416.

A blank license file was installed when I installed the software ?, I registered the evaluation copy via the Internet., but this just provided me with an activation key. Can you tell me why the license.dat file is blank ? and what can I do in order to be able to use this software ?

Thanks in advance,
ラベル(1)
0 件の賞賛
返信
1 解決策
2,219件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi there,

I would do the same answer as for the previous post:

the process has 2 phases:www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LICENSE

the second point allows you to activate your license, provide the required information and the licensing department will send you an evaluation license file.

Note: the linux tools per default come with and empty license.dat file... nothing to do with the licensing process, nothing to be worry about.

Hope this helps...

Regards


元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,220件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi there,

I would do the same answer as for the previous post:

the process has 2 phases:www.freescale.com/webapp/sps/site/overview.jsp?code=CW_LICENSE

the second point allows you to activate your license, provide the required information and the licensing department will send you an evaluation license file.

Note: the linux tools per default come with and empty license.dat file... nothing to do with the licensing process, nothing to be worry about.

Hope this helps...

Regards


0 件の賞賛
返信