Licensing for CW10.1 Special Edition for Kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Licensing for CW10.1 Special Edition for Kinetis

Jump to solution
4,670 Views
Niall
Contributor II

When I try to build a project in CW10_MCU_V10.1_SE I get a message saying my application could not obtain a license file. I though that the special edition did not require a license file.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,934 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Sorry for the late reply on this topic.

This issue is a known issue specific to the Kinetis build tools (therefore, only people building with those targets should experience this issue).  It will be addressed in future releases.

In the meantime, here is the best workaround:

Edit the "cwide-env" file which is located at: {install path}\eclipse\

Append the following line to the file (just use a text editor):

FLEXLM_BATCH= -add 1

View solution in original post

0 Kudos
Reply
7 Replies
2,935 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Sorry for the late reply on this topic.

This issue is a known issue specific to the Kinetis build tools (therefore, only people building with those targets should experience this issue).  It will be addressed in future releases.

In the meantime, here is the best workaround:

Edit the "cwide-env" file which is located at: {install path}\eclipse\

Append the following line to the file (just use a text editor):

FLEXLM_BATCH= -add 1

0 Kudos
Reply
2,934 Views
joker441
Contributor I

same here...

0 Kudos
Reply
2,934 Views
Niall
Contributor II

I would like to add some more information on my previous post. I have installed the Special Edition of CW10.1 for windows (CW10_MCU_V10.1_SE). When I try to build one of the Kinetis example projects I get a Flexnet License Finder error saying that a license can't be obtained. The screenshot is attached. My understanding is that the Special edition of Codewarrior does not need a registered license and that a license file is installed during installation. My installation directory does not contain a license.dat file.

 

Has anybody else come across the same problem? I am trying to figure out if it is an installation problem or a bug in the special edition.

0 Kudos
Reply
2,934 Views
moat
Contributor I

error still exists...

 

Downloading eval now.

0 Kudos
Reply
2,934 Views
kef
Specialist I

Did you see last post to this thread ?:

https://community.freescale.com/thread/80580

0 Kudos
Reply
2,934 Views
olebon
Contributor I

I am having the same problem. I guess it will never be solved :smileysad: The only solution is to remove this retarded CW and use IAR instead.

 

 

PS Just added "FLEXLM_BATCH= -add 1" to the eclipse config file, this helped. Decided to keep CW :smileyhappy:

0 Kudos
Reply
2,934 Views
emh203
Contributor II

I have experienced this too.   I amusing the evaluation edition for now....

0 Kudos
Reply