License problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
12,620件の閲覧回数
Simulator
Contributor I
I am installed CodeWarrior.
I am get the registry and authorisation code. and ETHERNET card
I get the license:
But, then I press to IDE icon I get
the next message:
THe license was not found, auth code was not found
No such future exist:
Win32_CWIDE_limited
Flexlm error -5,357

Please help me to open codeWarrior
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
6,823件の閲覧回数
CrasyCat
Specialist III

Hello

I would recommend you to send an email to our licensing department describing the problem and attaching the license file and information about the product you have installed.

Also if you can deliver tools information tat would be perfect.

To collect these information:

- Start a window explorer
- Browse for your installation PROG sub-directory
- Start linker.exe
- Select Help -> About
-     Click on the “Extended Information” button.
-      When text changes to “Added Information” all necessary data are available.
-       Copy whole content of the dialog box to a text file that you can send over to licensing.

CrasyCat

 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
6,823件の閲覧回数
CrasyCat
Specialist III

Hello

Which processor are you targeting (HC08, HC12, Coldfire, ...)?

Which version of CodeWarrior are you using?

CrasyCat

0 件の賞賛
返信
6,823件の閲覧回数
Simulator
Contributor I
I  installed  CodeWarrior 8
Development Studio MPC5XX Edition
and on disk is CW_EPPC 5XX_8.1

Thank you
0 件の賞賛
返信
6,823件の閲覧回数
CrasyCat
Specialist III
Hello
 
 For some reason you probably discard your original license.dat file.
 Can you please add the following line at the beginning of your license file (in
 your CodeWarrior installation directory):
 
FEATURE Win32_CWIDE_Limited metrowks 5.5 permanent uncounted \
       2589EF7E8174 HOSTID=ANY
 
This should allow you to at least open the IDE
 
CrasyCat
 

 
0 件の賞賛
返信
6,823件の閲覧回数
Simulator
Contributor I
Hi,
CrasyCat.
Thank you ,for help
But after registration
I get the
next file,that is not working.
That can I do with this license file?
We buy 10 licenses ,and no one of them worked.
 
 
FEATURE
                                                                 HI014150 HIWARE 2.0 permanent uncounted B8CD4F1481D0 \
 
       HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI040155 HIWARE 2.0 permanent uncounted 0555E7EE7A8D \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI040160 HIWARE 2.0 permanent uncounted FD4907CF10F9 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI040170 HIWARE 2.0 permanent uncounted F1D434B402FD \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044010 HIWARE 2.0 permanent uncounted 2172228AFC82 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044011 HIWARE 2.0 permanent uncounted 8327078208D6 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044012 HIWARE 2.0 permanent uncounted D41A006E9CE2 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044013 HIWARE 2.0 permanent uncounted 889925DE0836 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044014 HIWARE 2.0 permanent uncounted BBAA560A2CDA \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044015 HIWARE 2.0 permanent uncounted CF6DCB62180E \
       HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044016 HIWARE 2.0 permanent uncounted 8B8FD48EFC8A \
 
       HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044017 HIWARE 2.0 permanent uncounted 1980D96E28EE \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044018 HIWARE 2.0 permanent uncounted 4172AA7AAC32 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044019 HIWARE 2.0 permanent uncounted 3C254F9238C6 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044020 HIWARE 2.0 permanent uncounted 8872C71F064E \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI044021 HIWARE 2.0 permanent uncounted A89B2093FEEA \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI404000 HIWARE 2.0 permanent uncounted B88F89911236 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI404010 HIWARE 2.0 permanent uncounted 7C4DDA26B4B6 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI404020 HIWARE 2.0 permanent uncounted 3BE52F3B8EC2 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI404030 HIWARE 2.0 permanent uncounted 8053A89020CA \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI404050 HIWARE 2.0 permanent uncounted B28906EA94A6 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI404060 HIWARE 2.0 permanent uncounted 84EEEB6F5ED2 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI404100 HIWARE 2.0 permanent uncounted C5F3A5C568F5 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI404105 HIWARE 2.0 permanent uncounted 70711A1590D1 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI404220 HIWARE 2.0 permanent uncounted 49926F4386A8 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI415240 HIWARE 2.0 permanent uncounted B7B2FACD68CA \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI415245 HIWARE 2.0 permanent uncounted 577AE7D9E086 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
FEATURE HI491000 HIWARE 2.0 permanent uncounted 0A78B651AC18 \
 HOSTID=000d61604ee6 NOTICE=AAJC8-2E813-F313D-C686E
 

 
 
 
 
0 件の賞賛
返信
6,824件の閲覧回数
CrasyCat
Specialist III

Hello

I would recommend you to send an email to our licensing department describing the problem and attaching the license file and information about the product you have installed.

Also if you can deliver tools information tat would be perfect.

To collect these information:

- Start a window explorer
- Browse for your installation PROG sub-directory
- Start linker.exe
- Select Help -> About
-     Click on the “Extended Information” button.
-      When text changes to “Added Information” all necessary data are available.
-       Copy whole content of the dialog box to a text file that you can send over to licensing.

CrasyCat

 

0 件の賞賛
返信
6,823件の閲覧回数
alex_spotw
Contributor III
HI:

Did you copy the new licence file into the CodeWarrior folder (C:\Program Files\Metrowerks\CW xxxx )

This works for us.

Regards,

Alex
0 件の賞賛
返信
6,824件の閲覧回数
peg
Senior Contributor IV

Gee now Codewarrior is prophesying!!!

 

Sorry I am sure you meant feature :smileyvery-happy:

Peg

0 件の賞賛
返信