License Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,944件の閲覧回数
nikesh5383
Contributor I

mwcceppc.exe( processor Zen is not supported by the current set of licenses.
mwcceppc.exe( Please contact <[email protected]> for licensing needs

 

Following appears when i try to run a build. What could be the reason for such a message.

 

I have purchased a dongle and have the license installed.

 

How should i debug?

 

I dont use the complete Codewarrior IDE but only the compiler.

 

It worked well before with a floating license but now with the dongle it does not work. I even tried the evaluation version and that works absolutely fine.

 

Is there anything else i have to take care when using a dongle?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,204件の閲覧回数
J2MEJediMaster
Specialist I

Try this web page. It has the latest QuickStart Guide for dongle installation and the latest drivers.

 

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,204件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi nikesh5383,

 

I'd suggest you to check FAQ-27403:

 

http://www.freescale.com/webapp/sps/utils/SingleFaq.jsp?FAQ-27403.xml

 

It's dedicated to CodeWarrior for ColdFire, but it's applicable to Power Architecture CodeWarrior as well.

 

Does the licensing issue appear also in CW IDE?

 

Stanish

 

0 件の賞賛
返信
4,204件の閲覧回数
nikesh5383
Contributor I

i am unable to find anny info in the FAQ that you suggested. Kindly update.

0 件の賞賛
返信
4,205件の閲覧回数
J2MEJediMaster
Specialist I

Try this web page. It has the latest QuickStart Guide for dongle installation and the latest drivers.

 

---Tom

0 件の賞賛
返信