LM_VENDOR_DOWN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LM_VENDOR_DOWN

Jump to solution
8,900 Views
Takeo
Contributor II
 

I am using LS1012A.

CodeWarrior Development Studio for QorIQ LS Series -ARM V8 ISA causes LM_VENDOR_DOWN.

Please tell me how to deal with it. The environment is as follows.

 

1. I installed ARMv8ISA from the USB memory of CodeWarrior Development Suite.

2. Execute the update from Help

3. Execute "CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe"

4. Execute the update from Help After restarting, click HELP> NXP License to check the license status.

Product: CodeWarrior Debugger

Version: 14.0.202109301004

Status: Unknown error with key ARMv8DBG 11.0, LM_VENDOR_DOWN

"LM_VENDOR_DOWN" is also occurring in other products such as Trace Commander.

 

 

Regards, Takeo KOJIMA

0 Kudos
Reply
1 Solution
8,885 Views
Takeo
Contributor II

 

The situation has changed from the time of the previous posting, and the following license error occurs in NXP Licenses of CodeWarrior Development Studio for QorIQ LS Series -ARM V8 ISA (v2020.06).

Product CodeWarrior Debugger
Version 14.0.0.202109301004
Status Cannot find feature in the license file, error with key ARMv8DBG 11.0,

license.datファイルは以下を参照して作成しました。


https://community.nxp.com/t5/Software-Licensing-Knowledge/Floating-License-Environment-Variables/ta-...

 

ARMv8DBG in license.dat is as follows

INCREMENT ARMv8DBG metrowks 11.10 16-sep-2022 1 6709777E8542 \
VENDOR_STRING="CodeWarrior for QorIQ LS Series ARMv8 ISA" \
DUP_GROUP=UH ISSUER="Freescale Semiconductor" \
ISSUED=29-nov-2021 ck=68 SN="FSL - 36711427" TS_OK

Please tell me what to check

Regards, Takeo

View solution in original post

0 Kudos
Reply
4 Replies
8,886 Views
Takeo
Contributor II

 

The situation has changed from the time of the previous posting, and the following license error occurs in NXP Licenses of CodeWarrior Development Studio for QorIQ LS Series -ARM V8 ISA (v2020.06).

Product CodeWarrior Debugger
Version 14.0.0.202109301004
Status Cannot find feature in the license file, error with key ARMv8DBG 11.0,

license.datファイルは以下を参照して作成しました。


https://community.nxp.com/t5/Software-Licensing-Knowledge/Floating-License-Environment-Variables/ta-...

 

ARMv8DBG in license.dat is as follows

INCREMENT ARMv8DBG metrowks 11.10 16-sep-2022 1 6709777E8542 \
VENDOR_STRING="CodeWarrior for QorIQ LS Series ARMv8 ISA" \
DUP_GROUP=UH ISSUER="Freescale Semiconductor" \
ISSUED=29-nov-2021 ck=68 SN="FSL - 36711427" TS_OK

Please tell me what to check

Regards, Takeo

0 Kudos
Reply
8,877 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Can you please share the server logs, this means that the Deamon is not active.

0 Kudos
Reply
8,869 Views
Takeo
Contributor II
Jorge-san, Thank you for your reply, Log is , 17:18:28 (lmgrd) ----------------------------------------------- 17:18:28 (lmgrd) Please Note: 17:18:28 (lmgrd) 17:18:28 (lmgrd) This log is intended for debug purposes only. 17:18:28 (lmgrd) In order to capture accurate license 17:18:28 (lmgrd) usage data into an organized repository, 17:18:28 (lmgrd) please enable report logging. Use Flexera's 17:18:28 (lmgrd) software license administration solution, 17:18:28 (lmgrd) FlexNet Manager, to readily gain visibility 17:18:28 (lmgrd) into license usage data and to create 17:18:28 (lmgrd) insightful reports on critical information like 17:18:28 (lmgrd) license availability and usage. FlexNet Manager 17:18:28 (lmgrd) can be fully automated to run these reports on 17:18:28 (lmgrd) schedule and can be used to track license 17:18:28 (lmgrd) servers and usage across a heterogeneous 17:18:28 (lmgrd) network of servers including Windows NT, Linux 17:18:28 (lmgrd) and UNIX. 17:18:28 (lmgrd) 17:18:28 (lmgrd) ----------------------------------------------- 17:18:28 (lmgrd) 17:18:28 (lmgrd) 17:18:28 (lmgrd) Server's System Date and Time: Wed Dec 01 2021 17:18:28 ???? (?W?€??) 17:18:28 (lmgrd) pid 1980 17:18:28 (lmgrd) SLOG: Summary LOG statistics is enabled. 17:18:28 (lmgrd) Detecting other license server manager (lmgrd) processes... 17:18:31 (lmgrd) Done rereading 17:18:31 (lmgrd) FlexNet Licensing (v11.16.2.1 build 245043 x64_n6) started on 192.168.1.158 (IBM PC) (12/1/2021) 17:18:31 (lmgrd) Copyright (c) 1988-2018 Flexera. All Rights Reserved. 17:18:31 (lmgrd) World Wide Web: http://www.flexerasoftware.com 17:18:31 (lmgrd) License file(s): C:\flexlm\License Manager 64 bit\license (4).dat 17:18:31 (lmgrd) lmgrd tcp-port 27000 17:18:31 (lmgrd) (@lmgrd-SLOG@) =============================================== 17:18:31 (lmgrd) (@lmgrd-SLOG@) === LMGRD === 17:18:31 (lmgrd) (@lmgrd-SLOG@) Start-Date: Wed Dec 01 2021 17:18:31 ???? (?W?€??) 17:18:31 (lmgrd) (@lmgrd-SLOG@) PID: 1980 17:18:31 (lmgrd) (@lmgrd-SLOG@) LMGRD Version: v11.16.2.1 build 245043 x64_n6 ( build 245043 (ipv6)) 17:18:31 (lmgrd) (@lmgrd-SLOG@) 17:18:31 (lmgrd) (@lmgrd-SLOG@) === Network Info === 17:18:31 (lmgrd) (@lmgrd-SLOG@) Listening port: 27000 17:18:31 (lmgrd) (@lmgrd-SLOG@) 17:18:31 (lmgrd) (@lmgrd-SLOG@) === Startup Info === 17:18:31 (lmgrd) (@lmgrd-SLOG@) Is LS run as a service: Yes 17:18:31 (lmgrd) (@lmgrd-SLOG@) Server Configuration: Single Server 17:18:31 (lmgrd) (@lmgrd-SLOG@) Command-line options used at LS startup: -c C:\flexlm\License Manager 64 bit\license (4).dat -l C:\flexlm\License Manager 64 bit\log.log -z -s 17:18:31 (lmgrd) (@lmgrd-SLOG@) License file(s) used: C:\flexlm\License Manager 64 bit\license (4).dat 17:18:31 (lmgrd) (@lmgrd-SLOG@) =============================================== 17:18:31 (lmgrd) SLOG: FNPLS-INTERNAL-VL1-4096 17:18:31 (lmgrd) Starting vendor daemons ... 17:18:32 (lmgrd) Started metrowks (pid 3104) 17:18:32 (metrowks) FlexNet Licensing version v11.16.2.1 build 245043 x64_n6 17:18:32 (metrowks) SLOG: Summary LOG statistics is enabled. 17:18:32 (metrowks) SLOG: FNPLS-INTERNAL-CKPT1 17:18:32 (metrowks) SLOG: VM Status: 0 17:18:32 (metrowks) SLOG: FNPLS-INTERNAL-CKPT5 17:18:32 (metrowks) SLOG: TPM Status: 0 17:18:32 (metrowks) SLOG: FNPLS-INTERNAL-CKPT6 17:18:32 (metrowks) Invalid license key (inconsistent authentication code) 17:18:32 (metrowks) ==>INCREMENT CMSISDAP metrowks 11.10 16-sep-2022 1 75BA7FB23441 \ VENDOR_STRING="CodeWarrior for QorIQ LS Series ARMv8 ISA" \ DUP_GROUP=UH ISSUER="Freescale Semiconductor" \ ISSUED=29-nov-2021 ck=72 SN="FSL - 36711427" TS_OK 17:18:32 (metrowks) Invalid license key (inconsistent authentication code) 17:18:32 (metrowks) ==>INCREMENT FSLTAP metrowks 11.10 16-sep-2022 1 56C7D65935C2 \ VENDOR_STRING="CodeWarrior for QorIQ LS Series ARMv8 ISA" \ DUP_GROUP=UH ISSUER="Freescale Semiconductor" \ ISSUED=29-nov-2021 ck=66 SN="FSL - 36711427" TS_OK 17:18:32 (metrowks) Invalid license key (inconsistent authentication code) 17:18:32 (metrowks) ==>INCREMENT ARMv8DBG metrowks 11.10 16-sep-2022 1 6709777E8542 \ VENDOR_STRING="CodeWarrior for QorIQ LS Series ARMv8 ISA" \ DUP_GROUP=UH ISSUER="Freescale Semiconductor" \ ISSUED=29-nov-2021 ck=68 SN="FSL - 36711427" TS_OK 17:18:32 (metrowks) Invalid license key (inconsistent authentication code) 17:18:32 (metrowks) ==>INCREMENT PE_SCENARIOS metrowks 11.10 16-sep-2022 1 ED40C1B5590B \ VENDOR_STRING="CodeWarrior for QorIQ LS Series ARMv8 ISA" \ DUP_GROUP=UH ISSUER="Freescale Semiconductor" \ ISSUED=29-nov-2021 ck=159 SN="FSL - 36711427" TS_OK 17:18:32 (metrowks) Invalid license key (inconsistent authentication code) 17:18:32 (metrowks) ==>INCREMENT REMOTEDEBUG metrowks 11.10 16-sep-2022 1 FB59E7326545 \ VENDOR_STRING="CodeWarrior for QorIQ LS Series ARMv8 ISA" \ DUP_GROUP=UH ISSUER="Freescale Semiconductor" \ ISSUED=29-nov-2021 ck=93 SN="FSL - 36711427" TS_OK 17:18:32 (metrowks) License server system started on 192.168.1.158 17:18:32 (metrowks) No features to serve, exiting 17:18:32 (metrowks) EXITING DUE TO SIGNAL 27 Exit reason 4 17:18:37 (lmgrd) metrowks exited with status 27 (No features to serve) 17:18:37 (lmgrd) metrowks daemon found no features. Please correct 17:18:37 (lmgrd) license file and re-start daemons. 17:18:37 (lmgrd) 17:18:37 (lmgrd) This may be due to the fact that you are using 17:18:37 (lmgrd) a different license file from the one you expect. 17:18:37 (lmgrd) Check to make sure that: 17:18:37 (lmgrd) C:\flexlm\License Manager 64 bit\license (4).dat 17:18:37 (lmgrd) is the license file you want to use. 17:18:37 (lmgrd) 8:17:52 (lmgrd) TIMESTAMP 12/2/2021 Best Regards, Takeo Kojima
0 Kudos
Reply
8,326 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Can you schedule a call with me to solve the issue [email protected]

0 Kudos
Reply