KSZ9031 micrel PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSZ9031 micrel PHY

1,909件の閲覧回数
Tanushree
Contributor III

Hello all,

I'm working on a custom i.MX8DXL board in kernel version of 5.4.24. Ethernet is already worked in 5.15.52 with the same dts and board configuration. but porting back ethernet from 5.15.52 to 5.4.24 is not working.

Below is the dts file

&eqos {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_eqos>;
phy-mode = "rgmii-id";
phy-handle = <&ethphy0>;
fsl,magic-packet;
// nvmem-cells = <&fec_mac1>;
nvmem-cell-names = "mac-address";
snps,reset-gpios = <&lsio_gpio0 20 GPIO_ACTIVE_LOW>;
snps,reset-delays-us = <10 20 200000>;
status = "okay";

mdio {
compatible = "snps,dwmac-mdio";
#address-cells = <1>;
#size-cells = <0>;

ethphy0: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <1>;
rxdv-skew-ps = <480>;
txen-skew-ps = <480>;
rxd0-skew-ps = <480>;
rxd1-skew-ps = <480>;
rxd2-skew-ps = <480>;
rxd3-skew-ps = <480>;
txd0-skew-ps = <420>;
txd1-skew-ps = <420>;
txd2-skew-ps = <360>;
txd3-skew-ps = <360>;
txc-skew-ps = <1020>;
rxc-skew-ps = <960>;

};
};
};

pinctrl_eqos: eqosgrp {
fsl,pins = <
IMX8DXL_ENET1_RGMII_TXC_CONN_EQOS_RGMII_TXC 0x06000020
IMX8DXL_ENET1_RGMII_TXD2_CONN_EQOS_RGMII_TXD2 0x98000020
IMX8DXL_ENET1_RGMII_TX_CTL_CONN_EQOS_RGMII_TX_CTL 0x06000020
IMX8DXL_ENET1_RGMII_TXD3_CONN_EQOS_RGMII_TXD3 0x98000020
IMX8DXL_ENET1_RGMII_RXC_CONN_EQOS_RGMII_RXC 0x06000020
IMX8DXL_ENET1_RGMII_RXD3_CONN_EQOS_RGMII_RXD3 0x06000020
IMX8DXL_ENET1_RGMII_RXD2_CONN_EQOS_RGMII_RXD2 0x98000020
IMX8DXL_ENET1_RGMII_RXD1_CONN_EQOS_RGMII_RXD1 0x06000020
IMX8DXL_ENET1_RGMII_TXD0_CONN_EQOS_RGMII_TXD0 0x06000020
IMX8DXL_ENET1_RGMII_TXD1_CONN_EQOS_RGMII_TXD1 0x06000020
IMX8DXL_ENET1_RGMII_RXD0_CONN_EQOS_RGMII_RXD0 0x06000020
IMX8DXL_ENET1_RGMII_RX_CTL_CONN_EQOS_RGMII_RX_CTL 0x06000020
IMX8DXL_ENET1_REFCLK_125M_25M_CONN_EQOS_REFCLK_125M_25M 0x98000020
IMX8DXL_ENET0_MDC_CONN_EQOS_MDC 0x06000020
IMX8DXL_ENET0_MDIO_CONN_EQOS_MDIO 0x06000020
IMX8DXL_MCLK_OUT0_LSIO_GPIO0_IO20 0x600004c
>;
};

Config name is added

CONFIG_MICREL_PHY=y

0 件の賞賛
返信
1 返信

1,886件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

You are using NXP drivers and building micrel driver, try attaching it to a micrel PHY. This may be useful.

Regards

0 件の賞賛
返信