How do I activate evaluation license for MobileGTv9.2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I activate evaluation license for MobileGTv9.2?

2,893 次查看
danedmondson
Contributor I

I have downloaded and installed CodeWarrior for MobileGT for windows. When I try to start the IDE I get a dialog window saying the license is not valid. How do I use the eval app without a license? I have attached a screen copy of the error window.

标签 (1)
0 项奖励
回复
3 回复数

2,473 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

from your screenshot, there are two possiable reasons:

1. your evaluation is expired.

2. your CW doesn't recognize your license.dat file

please upload your license.dat file here. thus we can confirm if it belongs to first case. this file is under your CW install folder. thanks!

=================================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 项奖励
回复

2,473 次查看
danedmondson
Contributor I

Hello ZhangJun,

This morning I realized the problem is due to trying to run IDE through Remote Desktop. If I run directly from the laptop CW is installed on I do not get the license dialog. So I may not be able to run this remotely.

However, IDE will not start because the "preferences file is read only or currently in use". I have full admin permissions but cannot override the READ ONLY designation of the CW installed directories.

Here is the license file:

FEATURE Linux_CWIDE_Limited metrowks 5.5 permanent uncounted AB1FAA998915 HOSTID=ANY


INCREMENT Win32_CWIDE_Limited metrowks 5.5 permanent uncounted \
B966F84D1F0B HOSTID=ANY
INCREMENT Win32_Plugins_AXE metrowks 1.0 22-may-2014 uncounted \
0368F39F5F15 VENDOR_STRING="AXE CCS Protocol Plugin" \
HOSTID=ANY START=22-Apr-2014
INCREMENT WIN32_PLUGINS_DBG_AXE metrowks 1.0 22-may-2014 uncounted \
9DD68771BFE7 VENDOR_STRING="AXE Debugger plugin" HOSTID=ANY \
START=22-Apr-2014
INCREMENT WIN32_PLUGINS_GCC_Adapters metrowks 1.0 22-may-2014 \
uncounted D25A2F8AC812 VENDOR_STRING="GCC Adapters Windows" \
HOSTID=ANY START=22-Apr-2014
INCREMENT Win32_CWIDE_Unlimited metrowks 5.5 22-may-2014 uncounted \
2625109028F7 HOSTID=ANY START=22-Apr-2014
INCREMENT WIN32_PLUGINS_DBG_PPC metrowks 8.0 22-may-2014 uncounted \
DBDF496730A9 VENDOR_STRING="EPPC Debugger" HOSTID=ANY \
START=22-Apr-2014
INCREMENT Win32_PLUGINS_PPCCPU_MGT metrowks 8.0 22-may-2014 uncounted \
54DC0E4690F7 VENDOR_STRING="PPCCPU_MGT plugins (Windows)" \
HOSTID=ANY START=22-Apr-2014
INCREMENT Win32_PLUGINS_PPCCPU_COMM metrowks 1.0 22-may-2014 \
uncounted 1E11BD99D86E VENDOR_STRING="EPPC CPU_COMM" \
HOSTID=ANY START=22-Apr-2014
INCREMENT Win32_Plugins_Common_eLinux metrowks 2.0 22-may-2014 \
uncounted 9CD4478DDE0B VENDOR_STRING="EPPC CPU_COMM" \
HOSTID=ANY START=22-Apr-2014
INCREMENT Win32_Plugins_PPC_EmLinux metrowks 2.0 22-may-2014 \
uncounted 23C3C4F873B8 VENDOR_STRING="EPPC CPU_COMM" \
HOSTID=ANY START=22-Apr-2014
INCREMENT Win32_CFP_EPPC metrowks 8.0 22-may-2014 uncounted \
7E48434BAD47 VENDOR_STRING="EPPC Flash Programming" HOSTID=ANY \
START=22-Apr-2014
INCREMENT Win32_CFP_PPC metrowks 8.0 22-may-2014 uncounted \
6347965D9733 VENDOR_STRING="PPC Flash Programming" HOSTID=ANY \
START=22-Apr-2014
INCREMENT WIN32_PLUGINS_COMP_PPC metrowks 8.0 22-may-2014 uncounted \
C00E9B350658 VENDOR_STRING="PPC build tools" HOSTID=ANY \
START=22-Apr-2014
INCREMENT WIN32_PLUGINS_PPC metrowks 8.0 22-may-2014 uncounted \
CBA1FAF79B34 VENDOR_STRING="EPPC Plugins" HOSTID=ANY \
START=22-Apr-2014
INCREMENT Win32_Plugins_Link_PPC metrowks 8.0 22-may-2014 uncounted \
42D82BEDCECB VENDOR_STRING="PPC linker" HOSTID=ANY \
START=22-Apr-2014
INCREMENT ProcessorExpertMPC512x metrowks 1.000 22-may-2014 uncounted \
FBAAE1434BF0 VENDOR_STRING="Basic \
beans;2F16AA14EA8B12722D8ECEA2E975CA4A, Processor Expert \
MPC512x" HOSTID=ANY START=22-Apr-2014

0 项奖励
回复

2,471 次查看
stanish
NXP Employee
NXP Employee

Hello Dan,

attached is the temporary license valid until 30-may-2014 with the Terminal services licensing feature enabled ("TS-OK" parameter in license.dat).

Regarding preferences file the file that seems to be causing the problem lives here:

C:\Documents and Settings\\Local Settings\Application Data\Metrowerks

and is called:

  CodeWarrior IDE 5.x Prefs

  If  you right-click on this file and choose Properties, you can turn off the Read Only setting and then CW should work for you again.

Hope it helps.

Stan

0 项奖励
回复