Floating license connection error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Floating license connection error

4,010 Views
hansung_jung
Contributor III

I had used an evaluation version of CodeWarrior® Development Studio for HCS12(X), I purchased a license of CWP-STANDARD-FL-ND a few days ago.

I conducted registration and generated a license key of Development Studio for HCS12(X).

And then I set up the license server environment.

(referring to "FLTLICINSTWINBR.pdf", at the client-side, I pasted "license.dat" from the server and set system variable)

Host and client PC are combined through a local network.

However, I got this message, when I try to compile.

error.jpg

At that time, the license server's status is like below.

1.jpg

2.jpg

3.jpg

4.jpg

Labels (1)
0 Kudos
Reply
2 Replies

3,912 Views
stanish
NXP Employee
NXP Employee

Hi,

For debug this issue, please try to add [email protected] into LM_LICENSE_FILE environment variable.

CodeWarrior will first have a look there for the valid license before it checks the license.dat in the local folder.

Stan

0 Kudos
Reply

3,935 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

HI Hansung, 

it seems that the client machine is not connecting to the server, can you share a screen capture of the variable you created and also the location where the license file has been hosted on the client side.

Regards,

0 Kudos
Reply