Floating CodeWarrior license installed on the same PC as the CodeWarrior App

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Floating CodeWarrior license installed on the same PC as the CodeWarrior App

1,755件の閲覧回数
edwardjakob
Contributor I

I am working on an older project with a Freescale MPC8280 Power QUICC II.  We currently have two CodeWarrior floating licenses.

 

Is it possible to install a floating license on the same PC that hosts CodeWarrior itself?  It would make it easier if we would not have to network the two computers together to make CodeWarrior work.

 

The CodeWarrior Professional Suite - Perpetual was originally purchased by GE Aviation Systems in August 2009.  The registration codes are CWP-PRO-FL_1-566978505 and CWP-PRO-FL_1-566978512.

 

Thanks for any help you may have to offer.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,323件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Yes, you can install a floating license on the same PC that hosts CodeWarrior itself. The PC works as both Sever and Client.

Please also follow the instructions in this document to download and install floating license. The only difference is that the server and client are the same PC.

http://www.freescale.com/files/soft_dev_tools/doc/user_guide/CW_FLOA_LICEN_UG.pdf

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信