FlexLM server Licensing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexLM server Licensing

2,192 Views
stankogradev
Contributor I

- Do I have to delete the enviremental variable which points to the license server in order to release the license copy for use by other colleagues or the normal closing of the application is sufficient for the release of the license number ?

Labels (1)
0 Kudos
Reply
2 Replies

1,663 Views
trytohelp
NXP Employee
NXP Employee

Hi,

just an additional info.

By default the feature(s) is(are) pre-reserved some times (5mn) for the same client/user.

The feature(s) can not be use immediately by another customer during this time, even if the CodeWarrior was closed on First client.

After 5mn the feature(s) will be available for other clients.

the rule is defined in Flexlm manual as lingering time.

For CodeWarrior the default value is 5mn.

The user can not reduce this time but can increase it.

regards

Pascal

0 Kudos
Reply

1,663 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

yes, the normal closing of the application is sufficient for the release of the license number.