DLA-STANDARD-FL license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DLA-STANDARD-FL license

3,249件の閲覧回数
homereaton
Contributor I

Would like to run CodeWarrior using one computer at home and another one at the office but not concurrently. Is that possible with my FL license?

Homer

[email protected]

 

0 件の賞賛
返信
2 返答(返信)

3,245件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello, 

Yes, it can be possible as soon as the home computer is connected to the same network (same IP range) as the server. It can be through VPN but, if the connection is not good, it will fail. 

Best Regards, 

Paulina

0 件の賞賛
返信

3,237件の閲覧回数
homereaton
Contributor I

Thank you very much for responding, Paulina.

Always used NL license before, first time with an FL.  My license.dat file generated doesn’t work. Read a lot of help on this but never found the help in inputting the correct settings for "Server Name / IP Address" and "Port" Do I get these settings from IPCONFIG /ALL data? Would very much appreciate your help. Can send you the license.dat file if that helps.

Thanks,

Homer

0 件の賞賛
返信