Codewarrior - license server and client on the same machine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior - license server and client on the same machine

Jump to solution
4,140 Views
nad46
Contributor I

Greetings,

Young engineer here. Is it possible to have the license server on the same machine that will also be using the IDE? The Floating License Installation for Windows guide does not explicitly state that it is not allowed and I do not see why it would not work.

I figured a quick post in the support forums to confirm my assumptions before making a purchase with my company's funds might be a wise decision. This is a temporary solution as the use of CodeWarrior is needed immediately by a single individual (me), but more individuals will be joining and a dedicated license server will eventually be set up, which I will move the license server onto. Thanks!

Best,

-N

0 Kudos
Reply
1 Solution
4,122 Views
lisettelozano
NXP Employee
NXP Employee

Hi, 

Yes, the same computer can work as a server and client. 

Here are the links you need for the installers and the guide:

Floating installation guide: https://www.nxp.com/docs/en/brochure/FLTLICINSTWINBR.pdf

License manager installer: https://www.nxp.com/lgfiles/updates/FlexLM/License%20Manager%2064%20bit.zip

LMTools: https://www.nxp.com/lgfiles/updates/FlexLM/lmtools%20for%20Windows%2064-bit.zip

 

Paulina

View solution in original post

0 Kudos
Reply
1 Reply
4,123 Views
lisettelozano
NXP Employee
NXP Employee

Hi, 

Yes, the same computer can work as a server and client. 

Here are the links you need for the installers and the guide:

Floating installation guide: https://www.nxp.com/docs/en/brochure/FLTLICINSTWINBR.pdf

License manager installer: https://www.nxp.com/lgfiles/updates/FlexLM/License%20Manager%2064%20bit.zip

LMTools: https://www.nxp.com/lgfiles/updates/FlexLM/lmtools%20for%20Windows%2064-bit.zip

 

Paulina

0 Kudos
Reply