Codewarrior license problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior license problem

ソリューションへジャンプ
8,229件の閲覧回数
stefanorocca
Contributor II
Hello to all,
I purchased a CWA-PRO-FL codewarrior suite.
 
My PC is not a server: it is only a PC (windows XP professional based) connected to the internet via an ethernet card.
 
I tried to activate it: received the license.dat file and loaded it in the codewarrior directory.
When I run the program, I get the following error:
 
The CodeWarrior IDE is licensed and a valid license key was not found
Please contact ....
Network connect to THIS_HOST failed
The license file indicates THIS_HOST, and the server is not running on this host.
If it's running on a different host, THIS HOST sould be changed to the correct host.
Feature: Win32_CWIDE_Limited
License pat
 
Could my problem resides in the fact that my PC is not a server?
 
Stefano    
ラベル(1)
0 件の賞賛
返信
1 解決策
5,106件の閲覧回数
stefanorocca
Contributor II
Problem solved.
 
The Customer Support changes my license to a node locked (NL) version.
 
Stefano

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,105件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Stefano,

In fact you have purchased Floating License CodeWarrior suite. In contrast to nodelocked license which works only on one PC, floating license allows you to run licensed CodeWarrior development tool on any computer within a LAN network.

In order to use this license you have to configure your PC to be the licensing server. In doesn't metter that  it's the same PC where you will run CodeWarrior.

Attached instructions may help you to do it.

I'd suggest you to replace THIS_HOST string within your license.dat (SERVER line) by IP address or host name of your PC.

Stanish

Floating23.doc

Message Edited by t.dowe on 2009-10-06 09:07 AM
0 件の賞賛
返信
5,106件の閲覧回数
stefanorocca
Contributor II
Hello Stanish,
many thanks for the info.
 
Unfortunately, it doesn't solve the problem. Now I have the following:
 
The CodeWarrior IDE is licensed and a valid key was not found. Please contact ...
License server does not support this feature
FLEXlm error: -18,147
 
Stefano  
0 件の賞賛
返信
5,107件の閲覧回数
stefanorocca
Contributor II
Problem solved.
 
The Customer Support changes my license to a node locked (NL) version.
 
Stefano
0 件の賞賛
返信