Codewarrior - floating license reservation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior - floating license reservation

5,422 Views
michthom
Contributor II

Hi!

 

We currently have 2 floating licenses for Codewarrior 5.2 (HC12).

I would like to know if there is any mecanism that allow to reserve a floating license for some hours or a few days.

The purpose is to be able to use Cowarrior out of the network.

 

With some other compiler environment it is possible for example to get a token, and then unplug the computer from the network. The license remains active for the reserved period of time.

Of course during this period of time the license is no longer available for the other users.

 

Thanks,

 

Michel

Labels (1)
0 Kudos
Reply
4 Replies

4,930 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Michel

For borrowing, you need:

+ a floating license/license server

+ the license file needs to have the BORROW keyword

+ you need to follow a strict process for borrowing (see attached manual) FlexLM End user's guide, page 102 – 105.

And also FlexLm License Management, page 14 – 15:http://cache.nxp.com/files/soft_dev_tools/doc/user_guide/CW_FLEXlm_License_Management_UG.pdf

http://cache.nxp.com/files/soft_dev_tools/doc/user_guide/CW_FLEXlm_License_Management_UG.pdf 

And this thread should be helpful to you:

trying to use the borrow function but it never takes a license

I suggest to use USB dongles instead, this is easier and much user friendly.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,930 Views
michthom
Contributor II

Hello Fiona,

Thank you for the fast and complete answer.

Reading the FlexLM End User’s guide, it is specified that if we want to borrow a floating license the license.dat has to contain the keyword “BORROW”.

Our license.dat does not contain such a feature. Can we add it manually?

Regards,

Michel

De : TICS_Fiona <mailto:[mailto:[email protected]]>

Envoyé : jeudi 7 avril 2016 09:12

À : Michel Thomas

Objet : ( Pub )Re: - Codewarrior - floating license reservation

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Codewarrior - floating license reservation

reply from Xin Kuang<https://community.freescale.com/people/TICS_Fiona?et=watches.email.thread> in CodeWarrior Licensing - View the full discussion<https://community.freescale.com/message/632692?et=watches.email.thread#comment-632692>

0 Kudos
Reply

4,930 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Michel

Yes, our license team can manually update the license file. I would suggest summiting a case. It's better under Case process for private license details.

https://community.freescale.com/docs/DOC-330215

And I also sent you a temporary license for CW5.2 by email,  you can use it on any PC.

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 Kudos
Reply

4,929 Views
michthom
Contributor II

Hi Fiona,

Thank you for the answer.

I have submitted a question under the Case process as you suggested.

Regards,

Michel

De : TICS_Fiona

Envoyé : lundi 18 avril 2016 07:36

À : Michel Thomas

Objet : Re: - Codewarrior - floating license reservation

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Codewarrior - floating license reservation

reply from Xin Kuang<https://community.freescale.com/people/TICS_Fiona?et=watches.email.thread> in CodeWarrior Licensing - View the full discussion<https://community.freescale.com/message/635598?et=watches.email.thread#comment-635598>

0 Kudos
Reply