CodeWarrior Flash Programmer License

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior Flash Programmer License

1,755 次查看
justinjonas
Contributor III

I have a valid evaluation license which shows up when I open the 'Freescale Licenses' window in CodeWarrior.

177673_177673.PNGCWLicense.PNG

I am trying to run the Flash Programmer using gdb, and I get the following errors:

 

(gdb) source ../../gdb_extensions/flash/cwflash.py
Starting flash programmer services...
Starting local server...
Successfully started gdb server 127.0.0.1:45000.
Set gdb remote timeout to 7200
Connecting to target...
Using LS1012A SoC
Using CWTAP connected to local usb port
Using jtag speed 16000
Connecting to probe...
GTA: license checkout failed.
connection failed
Target connection failed. Please re-check the settings.

Processor: LS1012A
Probe: CodeWarrior TAP
//
Additional error details:
[GTA: license checkout failed]

Closing debugger server...
Error: fail to start flash programming services.

 

Can anyone help me to fix this issue?

Thanks for your help!

标签 (1)
0 项奖励
回复
0 回复数