CodeWarrior Classic EVAL - flex

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior Classic EVAL - flex

2,216 Views
stephen_george
Contributor I

Trying to EVALUATE the legacy CodeWarrior classic edition ( 6.3 ) and would like to test the flex licensing situation.

However I read through the FLEX setup guide, but when I try to generate the license for the EVAL version it does not offer me the page (and fields) to enter Server ID or FLEX ID while generating license.

I would like to test this setup, as our this version has to run on WinXP inside a virtual machine, so want to test flex licensing solution works before paying to flex license

Thanks

Steve

0 Kudos
Reply
1 Reply

2,109 Views
TomasPaez
NXP Employee
NXP Employee

Evaluation licenses do not need a dongle nor Server set up.

Evaluation license file are used in client base mode , this means the license file will work locally wit no need of external hw such dongle or server. 

if you want to evaluation please go to the next page

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t... 

if you would like to test a more specific scenario such as dongle based or server based create a support case in www.nxp.com/support 

0 Kudos
Reply