CodeWarrior 5.2 license question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior 5.2 license question

7,985 次查看
karlsl
Contributor I

Hi,

 

yesterday I have downloaded Codewarrior 5.2 win eval version for HCS9 with 30 days licence and use it to compile the program. I installed the program and use the default licence. When the program goes into the debug mode, the dialog box appears that says "Feature HI407284: HC12 ANSI-C debug is running in demo mode! ANSI-C modules are not loaded, limited to 32768 bytes of C code"

I thought the 30 days eval license covers unlimited size of code. what should I do?


thanks,

标签 (1)
0 项奖励
回复
9 回复数

6,361 次查看
trytohelp
NXP Employee
NXP Employee

Hi Carl,

Is there a problem with the default license file ?

It's possible.

Please can you share the license you're using ?

To get a temp license file please contact us using the Case system.

To submit your case into the new system, please follow below steps:

  1) Go to http://www.nxp.com/support/sales-and-support:SUPPORTHOME.

  2) On the bottom of the page under Submit New Issues, click Hardware & Software.

  3) Register with your business email to access NXP technical online support.

  4) A verification email will be sent to your account. Click the link embedded in that email to verify your access.

  5) On the NXP online support page, select Contact Support from the top menu and click “submit a new case” to start the process.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,357 次查看
karlsl
Contributor I

Hello,

please see the attachment for the default license. This is the license I get after I install the program. When I click "help" and then "License Authorization" in menu. I get the error dialog box, please see, error.jpg in the attachment.

This is a new installation, so I have not altered anything. yet, I get this message....

thank,

Carl

\

0 项奖励
回复

6,360 次查看
trytohelp
NXP Employee
NXP Employee

!Hi Carl,

The License Authorization is not used anymore.

The right way to active the product is to put the license.dat on the main installation folder.

I've checked the license file you sent with a project checking the license file and this license file is working fine on my side.

I got:

HI407284 (metrowks, 5.000): HC12 ANSI-C Debug ((27 days, 13-mar-2016), Single User License, ANY, UNREGISTERED)

HI407285 (metrowks, 5.000): HC12 C++ Debug ((27 days, 13-mar-2016), Single User License, ANY, UNREGISTERED)

To be running this license file must be placed in the main installation folder:

    E:\Freescale\CWS12v5.1\license.dat

Attached you will find the project example I used.

If you can not open it please check if the "Use Test-Based projects" is selected.

pastedImage_0.png

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,360 次查看
karlsl
Contributor I

Hi Pascal,

thanks for reply. I have clicked the debug mode and the error message is what I receive, see attachment. I am using Codewarrior 5.2. I thought the license I am getting is eval license.

Thank you,

\

0 项奖励
回复

6,360 次查看
trytohelp
NXP Employee
NXP Employee

Hi Carl,

Strange ... very strange.

I've performed some tests with your license file under my HC12 v5.2 installation and the debugger is working.

I don't have the error.

Please can you:

    - launch the debugger,

    - click on Help + About,

    - capture all information listed on the dialog message (scroll down).

Let me what is the windows OS used.

I've experienced some "similar" problem but it was linked to a floating license file but not with Eval one.


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,360 次查看
karlsl
Contributor I

Hi Pascal,

attachment is what you requested. debugger is working fine when the code I compile is small. the s19 file size is 74 kb. however, I get the dialog box I showed you yesterday when the code I compile is big. the s19 file size is 154 kb.

I am using version 5.2 and my OS is Win7 64bits. the MCU I am using is MC9S12XEQ512MAA.

thank you,

Carl

\

0 项奖励
回复

6,360 次查看
trytohelp
NXP Employee
NXP Employee

Hi Carl,

The info provided is not from the debugger but from the IDE which is not relevant for this license issue.

pastedImage_0.png

Attached you will find another project example.

This is using the Simulator.

Please can you check it ?

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

6,360 次查看
karlsl
Contributor I

Hi Pascal,

attachment is from the help section in debugger... below info is what I saved from the information in this dialog box. also, I don't see the attachment. please send again, thank.

Directory: D:\work related\FAW\FAW Programs\FAW_AUTOMATICEnvironment file: D:\work related\FAW\FAW Programs\FAW_AUTOMATIC\P&E_Multilink_USB.iniGENPATH=D:\work related\FAW\FAW Programs\FAW_AUTOMATIC\Sources;C:\Program Files (x86)\Freescale\CWS12v5.2\lib\hc12c\src;C:\Program Files (x86)\Freescale\CWS12v5.2\lib\hc12c\include;C:\Program Files (x86)\Freescale\CWS12v5.2\lib\hc12c\lib;C:\Program Files (x86)\Freescale\CWS12v5.2\lib\xgatec\src;C:\Program Files (x86)\Freescale\CWS12v5.2\lib\xgatec\include;C:\Program Files (x86)\Freescale\CWS12v5.2\lib\xgatec\libLIBPATH=C:\Program Files (x86)\Freescale\CWS12v5.2\lib\hc12c\include;C:\Program Files (x86)\Freescale\CWS12v5.2\lib\xgatec\includeOBJPATH=D:\work related\FAW\FAW Programs\FAW_AUTOMATIC\binABSPATH=D:\work related\FAW\FAW Programs\FAW_AUTOMATIC\binTEXTPATH=D:\work related\FAW\FAW Programs\FAW_AUTOMATIC\bin

Web: <http://www.codewarrior.com>LM_LICENSE_FILE=License File: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datApplication FLEXlm License Version: 2.000, 8.4aVendor daemon: metrowksETHERNET="9c4e36c947ed 9c4e36c947ed 9c4e36c947ec 3c970eb64707 005056c00001 005056c00008"HOSTNAME=Carl-PCDISK_SERIAL_NUM=44c41344HI407284 (metrowks, 5.000): HC12 ANSI-C Debug (HC12, checkout failed, demo mode: 1024 bytes of code, running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI407284License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".HI407285 (metrowks, 5.000): HC12 C++ Debug (HC12, checkout failed, demo mode: 1024 bytes of code, running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI407285License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".

Additional license information for all tools in the same directory as the executable:

File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\chc12.dll HI100300 (metrowks, 5.000): 5.000f HC12 Compiler ANSI-C (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100300License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100320 (metrowks, 5.000): 5.000f HC12 Compiler C++ Extension (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100320License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100330 (metrowks, 5.000): 5.000f HC12 Encryption (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100330License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100331 (metrowks, 5.000): 5.000f HC12 Encryption BSU (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100331License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100360 (metrowks, 5.000): 5.000f HCS12X Compiler ANSI-C (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100360License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100370 (metrowks, 5.000): 5.000f HCS12X Compiler C++ Extension (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100370License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\chc12.exe HI100300 (metrowks, 5.000): 5.000f HC12 Compiler ANSI-C (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100300License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100320 (metrowks, 5.000): 5.000f HC12 Compiler C++ Extension (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100320License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100330 (metrowks, 5.000): 5.000f HC12 Encryption (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100330License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100331 (metrowks, 5.000): 5.000f HC12 Encryption BSU (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100331License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100360 (metrowks, 5.000): 5.000f HCS12X Compiler ANSI-C (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100360License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100370 (metrowks, 5.000): 5.000f HCS12X Compiler C++ Extension (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100370License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\coverage.wnd HI040155 (metrowks, 5.000): 5.000f Coverage Component (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI040155License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\cxgate.dll HI150000 (metrowks, 5.000): 5.000f XGATE Compiler ANSI-C (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI150000License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI150020 (metrowks, 5.000): 5.000f XGATE Compiler C++ Extension (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI150020License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI150030 (metrowks, 5.000): 5.000f XGATE Encryption (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI150030License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI150031 (metrowks, 5.000): 5.000f XGATE Encryption BSU (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI150031License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\cxgate.exe HI150000 (metrowks, 5.000): 5.000f XGATE Compiler ANSI-C (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI150000License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI150020 (metrowks, 5.000): 5.000f XGATE Compiler C++ Extension (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI150020License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI150030 (metrowks, 5.000): 5.000f XGATE Encryption (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI150030License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI150031 (metrowks, 5.000): 5.000f XGATE Encryption BSU (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI150031License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\elfload.dll HI404281 (metrowks, 2.000): 2.000f HC05 ELF/DWARF Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI404281License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI406281 (metrowks, 2.000): 2.000f HC11 ELF/DWARF Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI406281License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI408281 (metrowks, 2.000): 2.000f HC16 ELF/DWARF Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI408281License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI411281 (metrowks, 2.000): 2.000f M·CORE ELF/DWARF Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI411281License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI415261 (metrowks, 2.000): 2.000f PowerPC ELF/DWARF Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI415261License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI020261 (metrowks, 2.000): 2.000f ST7 ELF/DWARF Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI020261License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI024251 (metrowks, 2.000): 2.000f ST19X ELF/DWARF Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI024251License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI419281 (metrowks, 2.000): 2.000f 8051XA ELF/DWARF Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI419281License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI022271 (metrowks, 2.000): 2.000f H8/500 ELF/DWARF Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI022271License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\hiload.dll HI404282 (metrowks, 2.000): 2.000f HC05 Hiware Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI404282License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI406282 (metrowks, 2.000): 2.000f HC11 Hiware Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI406282License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI408282 (metrowks, 2.000): 2.000f HC16 Hiware Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI408282License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI411282 (metrowks, 2.000): 2.000f M·CORE Hiware Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI411282License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI415262 (metrowks, 2.000): 2.000f PowerPC Hiware Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI415262License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI020262 (metrowks, 2.000): 2.000f ST7 Hiware Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI020262License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI024252 (metrowks, 2.000): 2.000f ST19X Hiware Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI024252License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI419282 (metrowks, 2.000): 2.000f 8051XA Hiware Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI419282License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI022272 (metrowks, 2.000): 2.000f H8/500 Hiware Loader (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI022272License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\linker.dll HI100050 (metrowks, 2.000): 2.000f HC05 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100150 (metrowks, 10.000): 10.000f HC08 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100150License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100250 (metrowks, 2.000): 2.000f HC11 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100250License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100350 (metrowks, 5.000): 5.000f HC12 Linker (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100350License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100450 (metrowks, 2.000): 2.000f HC16 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100450License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100550 (metrowks, 2.000): 2.000f M68k Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100550License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100650 (metrowks, 2.000): 2.000f M-CORE Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100650License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI105650 (metrowks, 2.000): 2.000f PowerPC Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI105650License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI120050 (metrowks, 2.000): 2.000f ST7 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI120050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI121050 (metrowks, 2.000): 2.000f ST19X Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI121050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI110050 (metrowks, 2.000): 2.000f 8051XA Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI110050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI150050 (metrowks, 5.000): 5.000f XGATE Linker (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI150050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI130050 (metrowks, 2.000): 2.000f i8051 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI130050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI140050 (metrowks, 2.000): 2.000f H8/500 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI140050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\linker.exe HI100050 (metrowks, 2.000): 2.000f HC05 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100150 (metrowks, 10.000): 10.000f HC08 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100150License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100250 (metrowks, 2.000): 2.000f HC11 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100250License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100350 (metrowks, 5.000): 5.000f HC12 Linker (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI100350License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100450 (metrowks, 2.000): 2.000f HC16 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100450License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100550 (metrowks, 2.000): 2.000f M68k Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100550License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI100650 (metrowks, 2.000): 2.000f M-CORE Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI100650License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI105650 (metrowks, 2.000): 2.000f PowerPC Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI105650License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI120050 (metrowks, 2.000): 2.000f ST7 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI120050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI121050 (metrowks, 2.000): 2.000f ST19X Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI121050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI110050 (metrowks, 2.000): 2.000f 8051XA Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI110050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI150050 (metrowks, 5.000): 5.000f XGATE Linker (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI150050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI130050 (metrowks, 2.000): 2.000f i8051 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI130050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com". HI140050 (metrowks, 2.000): 2.000f H8/500 Linker (running in demo mode(-5), UNREGISTERED)No such feature existsFeature: HI140050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -5,357For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\profiler.wnd HI040160 (metrowks, 5.000): 5.000f Profiler Component (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI040160License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\recorder.wnd HI404060 (metrowks, 5.000): 5.000f Recorder Component (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI404060License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\stimulation.wnd HI404050 (metrowks, 5.000): 5.000f Stimulator Component (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI404050License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".File name: C:\Program Files (x86)\Freescale\CWS12v5.2\prog\VisualizationTool.wnd HI404220 (metrowks, 5.000): 5.000f Visualisation Tool (running in demo mode(-88), UNREGISTERED)System clock has been set backFeature: HI404220License path: C:\Program Files (x86)\Freescale\CWS12v5.2\license.datFLEXlm error: -88,309For further information, refer to the FLEXlm End User Manual,available at "www.macrovision.com".

\

0 项奖励
回复

6,360 次查看
trytohelp
NXP Employee
NXP Employee

Hi Carl,

Flexlm generates the error: System clock has been set back.

The tool detected you modify the PC clock to an older date.

When PC clock is set back, the tool detects it and doesn't allow anymore to use evaluation or any time limited license file.

To unlock it you need a permanent license file.

Un-installing / Re-installing the tool doesn't solve the problem (info is in registry).

To solve the problem there are 2 solutions:

    - purchase a permanent suite,

    - re-install PC (Windows OS).

My example was included in previous post.

To access it you need to display the full message:

     CodeWarrior 5.2 license question

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复