CW Mobile V9.2 can't register with USB dongle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW Mobile V9.2 can't register with USB dongle

ソリューションへジャンプ
3,452件の閲覧回数
jettzhou
Contributor I

For the CodeWarrior for MobileGT V9.2, I start this software with plugging in the USB dongle, a message appears to say “no valid license key was found”(as follows  picture ).it seems the USB dongle has no use, but I had installed the usb driver and the dongle light is red .   I think that I had download the right license file from nxp website, and placed to the installed path.  So what is the reason ?  My computer config : 32 bit , win7 ;   (same problem in windows xp system)

ラベル(1)
0 件の賞賛
返信
1 解決策
3,103件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Jett Zhou,

We can only support USB dongle use on classic IDE releases using WinXP.  The Flex installers in the classic tools don’t play well with Windows 7 or newer. (this also applies to trying to use WnXP mode app)

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,104件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Jett Zhou,

We can only support USB dongle use on classic IDE releases using WinXP.  The Flex installers in the classic tools don’t play well with Windows 7 or newer. (this also applies to trying to use WnXP mode app)

Regards,

0 件の賞賛
返信
3,102件の閲覧回数
jettzhou
Contributor I

Hi

The customer try it.but it has the same error in winXP 32bit system.thanks.

B&R

Jett Zhou

MP: 15921091431

寄件者: jorge_plascencia

寄件日期: 2016年6月14日 4:36

收件者: Jett Zhou(周平生)(SHA)

主旨: Re: - CW Mobile V9.2 can't register with USB dongle

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

CW Mobile V9.2 can't register with USB dongle

reply from jorge_plascencia<https://community.nxp.com/people/jorge_plascencia?et=watches.email.thread> in CodeWarrior Licensing - View the full discussion<https://community.nxp.com/message/669637?et=watches.email.thread#comment-669637>

0 件の賞賛
返信
3,103件の閲覧回数
TomasPaez
NXP Employee
NXP Employee

It will be instersing to see the license file, - 5 error means the license file is not being seen by the application.

I dont see any license file on your account Jett, i will recomend to create a case to review the license file with the dongle ID

.  To submit your case into the new system, please follow below steps:

   1) Go to http://www.nxp.com/support/sales-and-support:SUPPORTHOME.

   2) On the bottom of the page under Submit New Issues, click Hardware & Software.

   3) Register with your business email to access NXP technical online support.

   4) A verification email will be sent to your account. Click the link embedded in that email to verify your access.

   5) On the NXP online support page, select Contact Support from the top menu and click “submit a new case” to start the process.

0 件の賞賛
返信