Activated license not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Activated license not working

1,940 次查看
denisdantas
Contributor II

Hello,

I currently have a paid license of the S12lisa toolchain but when I try to build our software, I get the following error:

"ERROR L4025: This limited version allows only 65536 bytes of C code"

When I open CodeWarrior and go to the Product Licenses window I can see that the license is activated (picture 1)

pastedImage_2.png

I also know that my makefile is linking to the correct license's path (picture 2)

pastedImage_3.png

In fact, the same project which I'm trying to build is being built by a colleague who also has the same license. I've been trying a few things to solve this but none worked so far. Any help on this issue will be very appreciated!

Best Regards,

Denis   

标签 (1)
0 项奖励
回复
3 回复数

1,662 次查看
stanish
NXP Employee
NXP Employee

Hello  Denis, 

This is indeed weird issue.

Could you please click on "Details" button and post the content here?

Can you attach also screenshot of  ERROR L4025 you get.

Thanks!

Stan

0 项奖励
回复

1,662 次查看
denisdantas
Contributor II

Issue solved. There was one environment variable missing.

0 项奖励
回复

1,662 次查看
stanish
NXP Employee
NXP Employee

Denis, Thanks for sharing the solution.

S.

0 项奖励
回复