secure element se051 revers current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

secure element se051 revers current

跳至解决方案
280 次查看
Devkun
Contributor I

 

I'm using  SE051 

I want to use the secure element feature to meet the Matter security criteria and the 14443A feature to implement Tap to Pair.

VIN Pin : in 3.3V DC Global net

Vout Pin pad to VCC Pin pad Connection.

SE051 switches on/off between VIN and Vout via the ENA pin.

When the switch is turned off, 14443a is activated..

Can the magnetically induced power from the NFC reader to the 14443 antenna affect the VIN?

Is the internal power switch of the SE051 protected against reverse current?

If this is not taken into consideration, can you suggest a solution?

Can I implement Matter's Tap to pair using SE051's 14443 feature?

 

 

 

 

 

 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
263 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Devkun ,

 

Can the magnetically induced power from the NFC reader to the 14443 antenna affect the VIN?

-No, it just supplies power to the same domain powered by VCC pin.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
264 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Devkun ,

 

Can the magnetically induced power from the NFC reader to the 14443 antenna affect the VIN?

-No, it just supplies power to the same domain powered by VCC pin.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
254 次查看
Devkun
Contributor I
Thanks for the quick feedback.
i have a one more question.
According to the datasheet of SE051
The chosen interface is the only interface the SE051 will receive commands for processing. To select a different interface the IC needs to be reset.

My question is : can a reset be performed by controlling the ENA pin, thereby changing the interface?

0 项奖励
回复