secure element se051 revers current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

secure element se051 revers current

ソリューションへジャンプ
264件の閲覧回数
Devkun
Contributor I

 

I'm using  SE051 

I want to use the secure element feature to meet the Matter security criteria and the 14443A feature to implement Tap to Pair.

VIN Pin : in 3.3V DC Global net

Vout Pin pad to VCC Pin pad Connection.

SE051 switches on/off between VIN and Vout via the ENA pin.

When the switch is turned off, 14443a is activated..

Can the magnetically induced power from the NFC reader to the 14443 antenna affect the VIN?

Is the internal power switch of the SE051 protected against reverse current?

If this is not taken into consideration, can you suggest a solution?

Can I implement Matter's Tap to pair using SE051's 14443 feature?

 

 

 

 

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
247件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Devkun ,

 

Can the magnetically induced power from the NFC reader to the 14443 antenna affect the VIN?

-No, it just supplies power to the same domain powered by VCC pin.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
248件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Devkun ,

 

Can the magnetically induced power from the NFC reader to the 14443 antenna affect the VIN?

-No, it just supplies power to the same domain powered by VCC pin.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
238件の閲覧回数
Devkun
Contributor I
Thanks for the quick feedback.
i have a one more question.
According to the datasheet of SE051
The chosen interface is the only interface the SE051 will receive commands for processing. To select a different interface the IC needs to be reset.

My question is : can a reset be performed by controlling the ENA pin, thereby changing the interface?

0 件の賞賛
返信