P71D600 naive code and JCOP ID2 platform - SDK/API/specifications ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P71D600 naive code and JCOP ID2 platform - SDK/API/specifications ?

3,584件の閲覧回数
PriwayEvaluation
Contributor I

We are evaluating a card based on the P71D600. Looking for SDK/API and lowlewel specifications - especially for NFC. Main object to evaluate if the chips can even handle our requirements.

In addition same on the JCOP ID2 - to determine if we have to go for native code.

I cant seem to locate the support information?

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

3,551件の閲覧回数
SecureElement
Contributor II

You can email me at [email protected]

0 件の賞賛
返信

3,575件の閲覧回数
SecureElementSolutions
Contributor I

You will have to contact an NXP FAE to get an NDA in place before they will release the specifications.  If I may ask, what is your specifications?

JCOP 4.5 is the latest OS and has a lot of options.  

One option is to use the JCOP OS and build SecureBox functions in native code that can be referenced from Javacard.  This saves you time so you do not have to build your own OS

3,556件の閲覧回数
PriwayEvaluation
Contributor I

a) Thanks. NDA in place, but it seems to be hard to get to the actual info.

b) New to the platform. Will look into this. It sounds like a model worth pursuing as we probably need very lowlevel aspects but certainly have no interest in building an entire OS.

0 件の賞賛
返信