P71D600 naive code and JCOP ID2 platform - SDK/API/specifications ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P71D600 naive code and JCOP ID2 platform - SDK/API/specifications ?

1,923 次查看
PriwayEvaluation
Contributor I

We are evaluating a card based on the P71D600. Looking for SDK/API and lowlewel specifications - especially for NFC. Main object to evaluate if the chips can even handle our requirements.

In addition same on the JCOP ID2 - to determine if we have to go for native code.

I cant seem to locate the support information?

标签 (4)
0 项奖励
回复
3 回复数

1,890 次查看
SecureElement
Contributor II

You can email me at mike@secureelementsolutions.com

0 项奖励
回复

1,914 次查看
SecureElementSolutions
Contributor I

You will have to contact an NXP FAE to get an NDA in place before they will release the specifications.  If I may ask, what is your specifications?

JCOP 4.5 is the latest OS and has a lot of options.  

One option is to use the JCOP OS and build SecureBox functions in native code that can be referenced from Javacard.  This saves you time so you do not have to build your own OS

1,895 次查看
PriwayEvaluation
Contributor I

a) Thanks. NDA in place, but it seems to be hard to get to the actual info.

b) New to the platform. Will look into this. It sounds like a model worth pursuing as we probably need very lowlevel aspects but certainly have no interest in building an entire OS.

0 项奖励
回复