Maximum input voltage of LA/LB of Desfire EV3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Maximum input voltage of LA/LB of Desfire EV3

424 次查看
alina
Contributor I

we have a customer use Desfire EV3, They ask the maximum input voltage of LA/LB , this parameter I did not find in datasheet. Could you help to check ? thanks a lot

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

234 次查看
thomas598henry
Contributor I

Hello @alina,
The maximum input voltage for LA/LB pins on Desfire EV3 isn’t explicitly listed in the datasheet. For precise electrical specs, it's best to contact NXP support directly or refer to their official community thread where similar queries are discussed.

Best Regards,
Thomas Henry

0 项奖励
回复

343 次查看
psvz
Contributor IV

Hi @alina 

Theory goes like this...

page 19 in MIFARE DESFire EV3 contactless multi-application IC gives us I-max of 86mA.

In a resonant LC circuit voltages on L and C are misaligned. I assume the ask comes from the need to assess calibrating capacitor rating, so let's deal with Vc.

VCmax = Imax * XC (capacitive reactance)

XC = 1 / (2 * π * f * C)

Assuming values 13.56MHz and 70pF, VCmax = 14.4V

I don't believe it is possible to guarantee anything here because an external reader outside your control drives the voltage - hence it can't be part of the specs.

 

0 项奖励
回复