when using MPXV6115VC6U with an arduino, do the additional capacitors and the resistor shown in fig 4 of the data sheet need to be used? what does "output source current operation" mean?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

when using MPXV6115VC6U with an arduino, do the additional capacitors and the resistor shown in fig 4 of the data sheet need to be used? what does "output source current operation" mean?

1,451 Views
robertprotin
Contributor I


i am trying to measure vacuum with an arduino and i just want to make sure i wont burn out the sensor

0 Kudos
Reply
1 Reply

1,160 Views
david_diaz
NXP Employee
NXP Employee

Hello Robert, 

They can be removed but I recommend using the configuration shown in the Figure 4 from the MPXV6115VC6U datasheet.

connection.jpg

The capacitors should avoid noise in both, input and output lines. The resistor was added to a scenario where several pressure sensors were connected to the same ADC input. 

Without these components, current would flow and give inaccurate results.

I hope this information will be useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply