vacuum pressure sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

vacuum pressure sensor

2,059 Views
cram1
Contributor I

I'm looking for a vacuum pressure sensor to control a process that operates at -2kPa from ambient atmosphere.

The temperature operating range is from +10 to +50C.

I'm looking for accuracy equal or better than 5%.

Labels (1)
0 Kudos
2 Replies

1,888 Views
lisettelozano
NXP Employee
NXP Employee

Hello Marc,

For your application, the best sensor will be the:

  • MPXV7002 Pressure range= -2 to 2kPa; temperature compensated over 10° to 60°C; 2.5% Typical Error over +10°C to +60°C with Auto Zero and 6.25% Maximum Error over +10°C to +60°C without Auto Zero.

Just in case that you can be interested in a higher pressure range, please see below:

  • MPXV7007DP Pressure range= -7 to 7kPa; Temperature Compensated Over –40° to +125°C and 5.0% Maximum Error Over 0° to 85°C.
  • MPXV70025DP Pressure range= -25 to 25kPa; Temperature Compensated Over –40° to +125°C and 5.0% Maximum Error Over 0° to 85°C.

I hope this information can be helpful.


Have a great day,

Paulina

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,888 Views
esehi123
Contributor I

i will go with MPXV7002, thanks a lot lisettelozano‌ mcdvoice

0 Kudos