pressure sensor MPX5100AP internal volume

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pressure sensor MPX5100AP internal volume

992 次查看
lars_wadso
Contributor I

I use MPX5100AP pressure sensors in a closed system where it is important that I know the system volume. To calculate that I need to know the internal volume of the sensor. Is this information available? If not, I have a question: can I fill an MPX5100AP with water (to assess the volume from the mass increase) without damaging the sensor?

标签 (1)
0 项奖励
回复
1 回复

862 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

It is ok to use water to calculate the internal volume of the MPX5100AP pressure sensor, just make sure that once the sensor is used for the final application, the internal cavity of the sensor has no residual of water and it is dry, otherwise could degrade the internal gel leaving the wire-bonds exposed and could cause shorts or internal corrosion.

 

You can probably use a couple of pressure sensors to get the measure of the internal volume of the sensor and use this values for the rest of the sensors without the need of introduce water into these sensors.\

Regards,

Jose

0 项奖励
回复